Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: TPS25750 Hi,
I have an adapter whose photo is attached below.
Thanks to this PD adapter, I can get various voltage and amperage values. I want to charge the battery by using 20V and 1.5A…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: AWR2243
Hello,
I'm a little bit confused about the describtion of the TX channels. The following graph shows that the TX channel of AWR#4 are 0 to 2 from left to right.
[mmWave Cascade Users…
Hi,
The cascade kit is composed of the following 2 items. You will need to buy these 2 items.
MMWCAS-DSP-EVM Evaluation board | TI.com
MMWCAS-RF-EVM Evaluation board | TI.com
You will also need to buy a Power Supply (not included in kit)
12V-5A Power…
Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: MMWCAS-RF-EVM Hi, we are working with the MMWCAS-DSP-EVM and the MMWCAS-RF-EVM and the PROCESSOR_SDK_RADAR_03_08_00_00. We are testing the Object radar detect usecase (it implements the MIMO…
Part Number: MMWCAS-RF-EVM Hi supporter;
We calibrate the phase mismatch between 4 cascade chips when TX power backoff=0.
After calibrated, we want to know if there will be phase mismatch when we set TX power backoff≠0.
thanks
Hi,
Yes the MMCAS RF EVM does support TX Beam forming, please refer the design guide of the EVM. https://www.ti.com/lit/pdf/tiduen5
The Typical TX power for AWR2243 device is 14dbm, however you will have to consider the Antenna Gain also for the total…
Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: AWR1243 Hello,
From D:\PROCESSOR_SDK_RADAR_03_08_00_00\vision_sdk\apps\src\rtos\radar\src\usecases\cascade_radar_object_detect\radar_cascade_demo.m
I understand that "4 AWR1243 Capture + Radar…