Part Number: TXS0104E Other Parts Discussed in Thread: TXS0102 , Hi, TI expert
The customer was considering TXS0102, but due to the added parts, he is considering TXS0104ERUTR, a 4ch product, for I2C/GPIO level conversion.
Here, I wonder if TXS0104E supports…
Part Number: TXS0104E Hi
What is the Maximum VCC current consumption when I operate all 4 channels in an Open-drain configuration @2Mbps speed?
VCCA - 1V8 and VCCB - 3V3 or 4V7.
Jebin
Part Number: TXS0104E Hello Sir:
Our application condition shows below.
Power up sequence is VCCB 3.3V > VCCA 1.8V
Schematic as below figure.
Also we saw that datasheet mentioning that OE pin needs to reference VCCA.
But our system power up sequence…
Part Number: TXS0104E Other Parts Discussed in Thread: TXU0104 , SN74AXC4T774 Hey,
I would like to use multiple TXS0104E in application where I have 1.8V signal output translated to 5V level, connected via cable to 1 or more TXS0104E as inputs. In the datasheet…
Part Number: TXS0104E
Hi,
The thermal pad (Pin# 15) was forgotten to be connected to the ground. We manufactured a few samples. It can cause a serious bug?
I will wait for your reply to connect to a power supply.
Thank you
Part Number: TXS0104E Hi
TXS0104EBQAR IC, OE pin is not connected (Open without pullup or pulldown). The IC shall be work as the OE="1", the IC has weak pullup
Thanks in advance
Part Number: TXS0104E Hi team,
One of my asia customer uses TXS0104E in an automotive application (Q1 not mandatory): do we have any safety documentation for the part? Ideally FIT, FMD and pin FMA documentation?
If you have safety doc for TXS0104E-Q1…
Part Number: TXS0104E Other Parts Discussed in Thread: PCF8575 , Hi,
I have a board with a processor and I2C pins that has to communicate with an IO-expander PCF8575. Since the I2C on the board uses 3.3V voltage and the PCF8575 uses 5V, there is a voltage…
Part Number: TXS0104E https://www.ti.com/materialcontent/en/search?partType=tiPartNumber&partNumber=TXS0104EYZTR
The provided report does not include any MDMS content. Could you please provide us with the MDMS report?
Part Number: TXS0104E Other Parts Discussed in Thread: TXU0102 , LSF0102 Hello TI support,
We are facing strange issue of RTC getting stuck during RF immunity testing with 20V/m field strength. We have some other product without use of level translator…