Part Number: TIDC-CC2650STK-SENSORTAG Other Parts Discussed in Thread: CC2650 , CC2650STK I have a Sensortag cc2650 device with BLE Rev 1.3.0. I want to interact with the optical sensor programatically. I want to know the values to be written to specific…
Hi Clement,
Thanks for your guidance, it works to make this profile_readSensor() in the task context, the advertising data is correct and ADC reading is also good. But there is one more question here:
1. With the notification of GATTServApp_ProcessCharCfg…
thank you for your reply
1.The BLE side writes 800 bytes to UART, the first 712 bytes received on the PC side are identical to the data sent by BLE; if BLE sends 200 bytes, the first 112 bytes are identical. The latter 88 bytes of these two cases are…
Part Number: LAUNCHXL-CC26X2R1 Hi,
I am using the basic ble example application on a CC26X2R1 Launchpad. I cofigured it to act in central role.
I managed to connect to the desired device.
I created the following function to read GATT characteristics: …
Part Number: INA220 Other Parts Discussed in Thread: INA237 , INA240 Hi,
We are using the mentioned P/N for current measurement with the following scheme:
The sequence we are using is pretty straight forward:
Setting Vout2_R to 9V -> Expected result…
Part Number: MSP430G2210 Other Parts Discussed in Thread: MSP430WARE Hi Experts,
Our customer wants to design one product which is Non-Rechargeable Battery Operated. Please help suggest ultra low power controller that can full-fill below requirements: 1…
Part Number: LAUNCHXL-CC26X2R1 Hi all,
I want to read SPI data and send through BLE with highest possible throughput, So I wrote my code based on Throughput Peripheral example.
In my code I use a timer for reading SPI and concept of dual buffer. When filling…
Part Number: LAUNCHXL-CC26X2R1 Hi, I'm working on BLE multirole project that facing an issue while trying to connect a peripheral device whenever the device range is below 5 meters means it's connecting more than 5 meter means connection not happen .…
Part Number: LAUNCHXL-CC2640R2 connections between 2 boards(CC2640R2) are happening, verified using putty serial monitor. I sent measured adc signal using simple_peripheral CC2640r2 , as instructed by this link,
https://dev.ti.com/tirex/explore/node?node…