Part Number: UA78 Hello guys,
One of my customers use UA7805CKTTR for their many mass-productions.
Recently, they received PCN which informs UA7805CKTTR will be discontinued. The PCN recommend to use LM7805SX/NOPB as a alternate device. But they checked…
Part Number: UA78 Other Parts Discussed in Thread: LM317 Hi, Dear Product line
our customer use UA7812 and UA7805 in their volume production but meet obsolete issue. so they select LM7812 and LM7805 from TI as alternatives. but customer has one concerns…
Part Number: UA78 Since there is a miswiring on UA7805 with external bias power of 5.5V - 6V into OUT pin of uA7805, customer would like evaluate if there is any risk. thanks.
What's the abs. max rating on OUT pin? thanks.
Regards
Brian
Part Number: UA78 Other Parts Discussed in Thread: LM317 Hi Team,
There is good news that we DIN UA7805CKTTR
But now customer need TO-252(DPAK) package
Do we have the solution
Part Number: UA78 Hi team,
Could you help me explain why UA7805 has 2 thickness package? (KCT and KCS)
Does some application need a thin package? or something.
thanks!
Part Number: UA78 Hi,
we are doing pin to pin replacement and find that both UA7805CKTTR and MC7805CD2TR4G are DDPAK package.
But MC7805CD2TR4G pin 2 is very short and seems not connected to any PCB copper, which is different from our device.
So I wonder…
Part Number: UA78
Hi, Does this LDO support -40℃? The absolute maximum rating is -65℃. However, the recommended operating temperature is 0℃. Could you tell me this reason? And Does this device get the following data? Customers want to know the relationship…