Part Number: UCC14240-Q1 Hi team.
Customer wants to change negative voltage value on the prototype like by mechanical-switch as below in order for checking supply voltage for SiC.
a. Vpos = 18V, Vneg = 0V
b. Vpos = 18V, Vneg = -5V
Do you have…
Qinghua,
Figure 5-10 from the UCC14240 EVM User Guide gives a picture of the inrush current during startup. You can see several peaks of current as high as 850mA and these are happening until the output voltage comes into regulation. The input voltage…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC15241-Q1 , UCC15240-Q1 Hi Team,
Do we have larger power isolated DCDC module? Customer need a 3W device. Thanks in advance.
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC15241-Q1 , UCC14241-Q1 , UCC15240-Q1 Hi,
I am looking at UCC14240-Q1 for a gate driver power supply application. I need -3/12V supply from a 24V input.
There is a contradiction in those…
Part Number: UCC14240-Q1 I'm trying to use it with the VDD-VEE 18V setting,but it can be 17.5V due to resistance variation.
Can it be used at 17.5V without any problems?
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC25800 , UCC14140-Q1 , UCC25800-Q1 Hi, The UCC14240-Q1 device uses a two switch "balancer-like" topology to regulate the COM-VEE voltage (Figure 7-2 in the UCC14240-Q1 datasheet). Does TI have…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC21750 , Hi, I am having some trouble with our UCC14240-Q1 implementation, we are using the UCC14240-Q1 in combination with the UCC21750 gate driver for a VSI design. In the picture below DPT…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: UCC14131-Q1 , UCC25800-Q1 Hi
Could you help suggest suitable products ,
Automotive displays must pass VSCC 56-3 The car power supply provides DC 24V, and the motherboard provides DC 12V.
…
Part Number: UCC14240-Q1 In the Rev. C datasheet Table 8-1 it says "For extreme input ripple voltage cases, connect a 4.75-ohm filter resistor to power input, PIN7, and connect a 10-μF ceramic capacitor from analog VIN PIN 6, to power analog GNDP." but…