Part Number: UCC21225A Other Parts Discussed in Thread: UCC27624 , UCC21520 Hi expert,
My customer used UCC21225A as functional isolation to eliminate the effect of ground bounce when hard switch off for their DAB topology.
And they connect the OUT to…
Part Number: UCC21225A Hi,
The voltage of the VCCI pin of UCC21225A is 9.5V, the voltage of the VDDA and VDDB pins is 11.2V, the Disable pin is connected to the ground, and the INTA and INTB pins provide input signals. The OUTA output is abnormal (no…
Part Number: UCC21225A Hi team,
For the bootstrap charging path, there is a confusing question that is looking for your support.
There is a situation that HS pin is not connected to Cboot Gnd, but the connection between HS PIN and Q1 source pin/SW node…
Part Number: UCC21225A Hi there,
customer need to know the input and output frequency range of UCC21225A.
what is the max and min frequency?
BRs,
Shubiao
Part Number: UCC21225A Other Parts Discussed in Thread: UCC21220 , UCC21222 Hi,
My customer is using UCC21225A but looking for another device in parallel because of the supply constraint. The smaller package is preferred. It looks for me UCC21225A is the…
Part Number: UCC21225A
Hi,
We are using this isolated driver ( UCC21225A) in shunt pwm dimming for led string. LED's are driven by constant current source Representative schematics attached
1) Here the series regulator never get reverse biased , since…
Part Number: UCC21225A Hi Team,
When my customer tried to power up with output load, it shows that the output signal of UCC21225 is not synchronous with input-signal DSP.
Please see this reference below:
I hope to hear from you soon, thank you.