Part Number: UCC27324 Other Parts Discussed in Thread: UCC28950 , Hello,
My name is Doğu Bora Yalçın, and I am employed as an Analog Design Engineer at ASELSAN. Presently, we are utilizing the UCC27324 Non-Inverting 4-A/4-A Dual-Channel Low Side Gate Driver…
Part Number: UCC27324 HI team, ESD rating has been changed from 4000V to 2000V due to a revision change in the datasheet. Is this due to the IC being weaker due to the process change? BR, Kengo.
Part Number: UCC27324 Other Parts Discussed in Thread: UCC28950 , , UCC27624 Hi Team,
The reference design in the customer's UCC28950 specification. The board only supplies the chip (UCC28950 and UCC27324) with 12V voltage, and the mos tube has not yet…
Part Number: UCC27324 Other Parts Discussed in Thread: LM5111 , , UCC27624 hi team,
my customer is using UCC27324 as a second source of LM5111, but the layout of LM5111 has been fixed with NC pins floating.
so can our UCC27324 NC pins be left floating?…
Part Number: UCC27324 Dear Specialists,
My customer is considering UCC27324 and has questions.
I would be grateful if you could advise.
---
(1) According to the latest data sheet (Rev.J) of UCC27324, the maximum value of TD2 in the switching characteristics…
Part Number: UCC27324 Hi team,
Customer has some questions
The device with UCC27324D model has a power supply voltage range of 4.5-15V. When testing VOH, 10mA is required. When the power supply voltage is 4.5V, the VOH value is lower than the lower limit…
Part Number: UCC27324-Q1 Other Parts Discussed in Thread: UCC27324 Hi experts,
How to understand the spec "output resistance high" in datasheet? It is 43R in datasheet, in this way, the max pull up driver capability will be 14V/43R=0.32A, it…
Part Number: UCC27324 Other Parts Discussed in Thread: UCC5320 , UCC23513 Can UCC27324 drive the SiC IC?
Do you have any actual results for this?
If it cannot drive SiC IC, can you recommend the right device that can drive SiC for this?
Part Number: UCC27324 Hi expert,
As this device is a dual channel driver, would like to learn below:
1. Are these two channels fully independent to operate? No any logic limitation for PWM input and output, right?
2. If two channels are used in parallel…