Part Number: UCC27511A Hi TI,
I built a half-bridge buck converter as shown below using EPC2031 switch and UCC27511A as driver for both high side and low side switches.
For the low side gate driver the ground node is connected to the power ground (GND…
Part Number: UCC27511A-Q1 The driver UCC27511AQ was damaged whenever the PFC voltage of 390V builts up (whenever IC comes into action which is above 65V output ) Mainly PIN 1 (VDD) and PIN 2((out1) tracks were damaging. Is there anything to do with the…
Part Number: UCC27511A-Q1 I require the lib file for
UCC27511A-Q1 as i need to model the gate driver in SABER, if any gate driver resembling this part , you can also share.
Part Number: UCC27511A Hi,
Good Day. I have a customer who is working with UCC27511A. Please see below his query for you reference. Thank you very much.
It would be possible to keep the OUTH pin of UCC27511A in high state indefinitely?
I am driving a…
Part Number: UCC27511A Other Parts Discussed in Thread: UCC27511 , UCC28070 HI TI team
I design 1200W that using PFC (ucc28070) and drive ic (ucc27511) I found that when the load is between 0 and 300W, AC instantly switches from 90Vac to 264Vac or from 264Vac…
Part Number: UCC27511A-Q1 Other Parts Discussed in Thread: UCC5350-Q1 Hello,
I have to design the High Voltage (800V) Heater System using Low-Side Switch circuit with IGBT
This system is similar to PTC Heater for HVAC.
https://www.rohm.com/documents/11303…
Part Number: UCC27511A Hi Team,
Please help me answer the follow question from my customer, thank you so much.
As I driven Nch MOS-FET with circuit like attached. There was a problem that the output of UCC27511A was damaged. The output pin is shorted to…
Part Number: UCC27511A Hello!
Can you make a statement about the capacitance on the inputs of UCC27511A ?
It seems not to be part of the datasheet. However, my customer wants to add an r-c filter to adjust interlock time. Ideal would be data over temperature…
Part Number: UCC27511A Hi team,
A customer is looking for a gate driver for an 80W HF application at about 40MHz. So they are looking for a small bandwidth, high power gate driver. Can you recommend a part?
Thank you,
Franz