Hi Aditya,
I understand the case that the external MOSFET is not damaged, and it is the internal MOSFET that is damaged.
However, I want to try to debug more in the case that there is more damage. Can you conduct a diode test from VDD to OUT and from OUT…
Hi Revathi,
Since it's been almost a month with no activity, I am assuming the problem has been solved, so I will be closing the thread. Feel free to reply to reopen if you have any issues.
Thanks, Rubas
Part Number: UCC27517A
I am using UCC27517A as gate drivers for high side and low side mosfets.
1) For the High side mosfet, the HS pin is connected to GND and IN- of UCC27517A. As the HS pin is switching node and 400V appears on it , can IN- and GND…
Part Number: UCC27517A Other Parts Discussed in Thread: UCC27511 , LMG1020 , UCC27614 Team,
My customer needs max/typ/min source/sink current at VDD=5V, since datasheet describes +/- 4A as typical at VDD=12V. Could you please clarify?
Best regards,
Ko…
Part Number: UCC27517A Other Parts Discussed in Thread: UCC27517 Hello all,
I have designed a simple circuit to turn on/off a MOSFET using the UCC27517 gate driver. The schematic is below.
Using a waveform generator, I am applying a pulse signal with…
Part Number: UCC27517A Other Parts Discussed in Thread: UCC27517 , UCC27531 , LM5114 , UCC27614 Customer is working on >700W Motor Drive system and the 3phase inverter is using stand-along GaN FET.
Vgs=6V, Frequency=50KHz
We're considering of ISO7710DR…
Part Number: UCC27517A Other Parts Discussed in Thread: LMG1020 , UCC27614 Hi team,
My customer is using our UCC27517A now.
And they wonder if we have a newer device to recommend.
Requirements:
4-A Peak Source and Sink
Fast Propagation Delays
Fast Rise…
Part Number: UCC27517A Other Parts Discussed in Thread: UCC27511 , PMP9656 , , UCC27611 , UCC27511A , PMP7451 , PMP3162 , PMP9720 , UCC27517 , UCC27614 Hi team,
For PMP9656, could we use the UCC27517A to replace the UCC27511?
We saw that UCC27517A is with inventory…