Part Number: UCC27524A1-Q1 Dear team,
When my customer use RθJC(top) listed in our datasheet to calculate Tj, Tj will be larger than 150C, so they hope we can help evaluate the actual RθJC(top) value based on their dissipation model as below. They…
Part Number: UCC27524A1-Q1 Hi
The customer uses this driver, and there is a waveform jitter in the driving voltage. The control signal is a 50% duty cycle square wave of 160KHz. Please refer to the attached MOS transistor data manual。 Infineon-IPW65R050CFD7A…
Part Number: UCC27524A1-Q1 Hi team:
Q1:We have test the current from OUTA of UCC27524A1-Q1. As shown in the following figure,the voltage of the 1ohm resistance was measured of which the value is equal to the output current.The peak value is 0.438A,could…
Part Number: UCC27524A1-Q1 Other Parts Discussed in Thread: DRV8245-Q1 Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "VNQ7050AJTR" ?
https://www.st.com/resource/en/datasheet/vnq7050aj…
Part Number: UCC27524A1-Q1 Hi team,
Which current does "500-mA reverse current without either damage", which is written in its datasheet "8.3.4 Output Stage", mention and why should this limitation be considered?
UCC27524A1-Q1 could…
Part Number: UCC27524A1-Q1 Hi team,
My customer refer to this post, and he wants to know :
1,What affect does the PI coating have on the part ( UCC27524A1-Q1) ? What aspect of the part does it improve (performance, quality, reliability, durability, etc…
Part Number: UCC27524A1-Q1 Other Parts Discussed in Thread: UCC27524 , UCC27531 I am currently using an IXYS ixdi604si gate driver. This driver has a different Power Supply Current depending on the input voltage as shown in data sheet.
I could use the…
Part Number: UCC27322-Q1 Other Parts Discussed in Thread: UCC27322 , UCC27524 Hallo all
I have a question about propagation delay. I find it difficult to estimate the propagation delay of this device.
When I compare UCC27322 with UCC27524A1, the propagation…
Part Number: UCC27524A1-Q1 Hi team,
Its "Absolute Maximum Ratings" says that "Output pulsed source/sink current (0.5 µs)" is 5A. Does it mean its output pulse (0.5us) current should be lower than 5A?
In addition, "Electrical…