Part Number: LM5146-Q1 Other Parts Discussed in Thread: LM5146 , , UCC27712 , LM5143-Q1 , LM5145 , LM5117-Q1 Hi team,
My customer has an application question regarding DEMB function of the LM5146-Q1 when external driver is used. My customer wishes to…
Other Parts Discussed in Thread: UCC27712 Hi, I have to control the speed of an AC motor and I need some reference design and guidelines to design my own speed controller for an AC motor. Right now, I have a 110V AC motor but it would be better if I can…
Hi Yoram,
I am sorry that you found my answer unacceptable and I appreciate your sincere feedback.
From your application description, it looks like you're trying to simulate a full topology using LM5114 (which is a low-side driver suited for different…
Hi Santhibhushan Addagarla,
I think that the IC given in the link of the previous post should be suitable for your needs. You will however need to use an external low voltage supply to power the device. You will also need to use an external driver that…
Part Number: UCC28780 Other Parts Discussed in Thread: UCC27712 Hi,
I am currently working on a Active Clamp DC-DC Flyback Converter based on UCC28780 and UCC27712. If I succeed we will use this topology and components in various designs. But I am struggling…
Hello Wim,
Thank you for the interest in the UCC27712. This is an interesting question that I have not seen requested before.
The mass of the UCC27212DPR package is 0.039G. Please confirm this is the part number and package of interest.
Regards…
Part Number: UCC27714 Other Parts Discussed in Thread: UCC27712 , , , UCC27712EVM-287 , UCC27212 Hello team,
Hope you are doing well. Please see below question from the customer:
I prototyped using the UC27714. For proof of concept, I used 2 of the…
Other Parts Discussed in Thread: UCC27712 , UCC27712EVM-287 , UCC27714 Derek,
Very good explanation, that makes sense. Now, can you provide the same explanation on the UCC27712 EVM-287? Page 9 of the user guide instructs to turn on the input power (0…