Part Number: UCC2805 Other Parts Discussed in Thread: UCC2813-5 Hi,
Good Day.
Customer would like to ask you a few questions that arise in the framework of a new design that currently is being developed.
The new PSU design is indented for automotive…
Part Number: UCC2805-Q1 Other Parts Discussed in Thread: UCC2805 , UCC2801 , UCC2803 , UCC2802 , UCC2804
Hi Expert,
UCC2805-Q1 was used on customer side. When they configure frequency based on the formula in datasheet. The resistor is 15k, and the capacitor…
Part Number: UCC2805 Dear team,
Customer has several question about ucc2805:
1. As the start-up current is very small, R491 should be tens of K Ohm, but I found that only Vin 12V, R491=2k that the system could power on normally. But if R491 is small…
Part Number: UCC2805-Q1 Other Parts Discussed in Thread: UCC2805 I have a question regarding the UCC2805 Over Current function. Since the COMP pin is clamped at 1V when the secondary output is in an over-current state, the PWM is always reset when CS reaches…
Part Number: UCC2805-Q1 Hi Expert,
The engineer is using the UCC2805-Q1.
Pls help to clarify the question about frequency behavior.
They are setting 100kHz from (10k +1000pF) on RC pin.
The results is 100khz on output pin and 200khz on RC pin.
Pls advice…
Part Number: UCC2805 Dear Teams,
My customer is using UCC2805. Could you help them solve following doubts?
Vin: 8-32V
1. How to remove the auxiliary winding due to limited space of transformer.
2. Could customer us the Vout (10V) as the supply voltage…
Part Number: UCC2805 Hi,
I have to simulate UCC2805 in Altium Designer. I begine with unencripted model that I found at TI web page.
Due to syntax issues I modified an simmulation do not retur any error anymore, component is not working.
Below I am sending…
Hi,
The same datasheet
https://www.ti.com/lit/ds/symlink/ucc3805.pdf?ts=1692009532292
If you look at Section 8.5, oscillator, and UCC2805 note (2) you will see:
"(2) Oscillator frequency for the UCCx800, UCC2802, and UCC2803 is the output frequency. …