Part Number: UCC2813-1 Hello. Datasheet has parameters for "Current sense"(page 6). Which element on the Block diagram (page 9) do these parameters refer to?
Thanks
Part Number: UCC2813-1 We got a problem with accurate calculation/simulation of UCC2813-1 oscillator frequency.
We found that the frequency from formula 1 (datasheet) is perfectly coincide with simulation but does not coincide with Fig.18 (datasheet…
Part Number: LM5168-Q1 Two times 5V are needed with one being isolated. For single output I could use 68 uH TYS6045680M or similar.
I'm not familiar with FlyBack transfomers. Which specific part is recommended in this case to replace the simple inductor…
Hi Srikar,
I am very sorry for the delay. I've given an overall response to your questions below after further discussion internally.
The most optimal solution (and to answer your second question) would be to organize the data movement as the fol…
Hello Sudhir, Can you please read the GPIOs and confirm they are in the correct state?
Above is an image of the GPIOs and what they are used for. Please be sure that they are not set to the wrong setting.
Best,
Quentin
Part Number: TLIN1029-Q1 Other Parts Discussed in Thread: TLIN1029A-Q1 , Hi team, The Figure 9-1 on p.22 of the datasheet is broken. https://www.ti.com/lit/ds/symlink/tlin1029-q1.pdf Are there any plans to fix this? And, is the correct picture the same as TLIN1029A…
Part Number: BQ79600-Q1 We use Infineon TC377 as the host and t he output state of the MOSI pin is determined by the state of the last bit of data sent by the host.
According to BQ79600 datasheet, master shall always drive MOSI to ‘1’ when not sending command…
Hi Martin,
Our RTC, BQ32000 and BQ32002 use crystal.
In fact, 32.768kHz TCXO is not a common part, only SiTime has products but it is MEMS but not crystal based.
Hi Kevin/Adam, Recommendation was to set Bit 31 of register address for PLL 7 = 0x687020
Can you measure power after the above PLL7 bypass setting and see if that is good enough for you?
- Keerthy