Part Number: UCC2813-4 Hi, I just designed a fly-back DC-DC converter with UCC2813-4. But it seems not work in high efficiency.
I checked the waveform and found that the duty cycle is only about 29%. At the same time, there's no current flow through the…
Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1860 Hi expert,
From the Datasheet , we want to kown PCM1860-Q1 Support 4 channel or 2 channel?
Below the picture, we think it support 4channel.
But Below the picture, it seems just support 2…
Part Number: TDA4VH-Q1
Hi experts,
I'm trying to display 4 RGB images using multi-display or mosaic.
The data flow is image->cv::mat->vx_image_RGB->display.
However, for multi-display, there are only 2 display to use (TIVX_TARGET_DISPLAY1…
Part Number: TCAN1044V-Q1 Other Parts Discussed in Thread: TCAN1044AV-Q1 , Hi TRX team,
Could you provide test result of IEC 61000-4-2 for TCAN1044VDRQ1? My customer requests that data.
Kind regards,
Shota
Part Number: DS90UB662-Q1 Hi team,
Hope you are doing well!
I have two CSI2 bandwidth calculation tools, V2.2 and V2.3, but the calculation results are not consistent, so I am not sure whether I can use DS90UB662-Q1.
1. This is the calculation result…
Part Number: TPS25772-Q1 Other Parts Discussed in Thread: TPS55288 , Hello,
I am designing a 4 port USB-C PD system for a vehicle, I am using TPS25772 + TPS55288, and was not able to understand the proper method for firmware updating. I see it can be done…
Hello Cao,
cao qi said: The GPIO 4 is connected to 3.3V through a 10K pull-up resistor. And o nly one board has this problem, so we suspect it may be a chip problem.
I am not ruling that out, but I find that is unlikely, could you send me in private a message…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com. when I click on the transformer, its showing popup with transformer information as CUSTOM…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com.
Another clarification required. you said NS1 is secondary and NS2 is auxillary. But the winding…