Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com. when I click on the transformer, its showing popup with transformer information as CUSTOM…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com.
Another clarification required. you said NS1 is secondary and NS2 is auxillary. But the winding…
Part Number: TPS65219-Q1 Hi Team,
For other platforms such as ST Accord 5 (L5964Q), can you recommend more commonly used specifications with stable supply for reference?
(1)VIN range: automotive Vbatt 12V/24V (or low voltage 5V is also acceptable) (2)LDO…
Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424E Hi team,
Could you please advise if all channels are enabled or 1 of 4 channel only enabled for Datasheet Figure 7-5. Output Power vs Supply Voltage?
I would like to drive TAS6424E under…
Part Number: UCC2813-5-Q1 Other Parts Discussed in Thread: TLV3501 Hi Team,
Our customer encountered an error when he imported the unencrypted PSpice model of UCC2813-5-Q1 to LTspice. The model is not working, showing too many nodes in the simulation as…
Hi Cao
The SD logs which you share i that we can see that you are getting communication error in U-BOOT for the emmc init .
cao qi said: Net: Could not get PHY for ethernet@46000000port@1: addr 0 am65_cpsw_nuss_port ethernet@46000000port@1: phy_connect(…
Part Number: LM7480-Q1 Hi Team,
Do we have any test result of LM74xx-Q1 in ISO7637-2 pulse 5b, load dump?
Customer want to see if the pulse is suppressed by LM7480-Q1, how low the Us can decrease.
They wonder if 30V or 26V device can be used after LM7480…
Part Number: DS90UB953-Q1 Hi team,
I have asked an E2E before about how to improve the robust of the link: (1) DS90UB953-Q1: Register to improve the robustness - Interface forum - Interface - TI E2E support forums
Customer only had 9530x52[1] error about…