Hi Harish,
Thank you for the swift reply.
I could not get the datasheet for RLTI-1100.
Regarding the 750344527, it does not meet the power requirement of 150W. I see that it has two secondary output 20V, 5A and 16V, 150mA. Can I connect it in series…
Part Number: UCC28600 Hi,
Compliment of the season!
Could you help me with an alternative boost inductor (L2) used in the UCC28600 120-W Evaluation Module. I cannot find the L2 listed on the BOM .
Also could you please confirm that the attached picture showing…
Part Number: UCC28600 Hi team,
Can non-isolated complex feedback be used with the UCC28600? No optocoupler is used.
If so, can you provide a reference design?
Part Number: UCC28600 Hello expert,
We are using UCC28600 aux_secondary.pdf for aux power supply 24V output. Input is from 200VDC to 1000VDC. We've modified REF_62W_FLY_1700V_SIC to have only single 24 V output. But the device shuts periodically with…
Part Number: UCC28600 Hello,
We need to build a 3 phase 8KV Surge Protection Circuit using UCC28600DR, So please provide us circuit diagram for this.
Thank You
Part Number: UCC28600 Other Parts Discussed in Thread: UCC28501 , UCC28051 , I'm planning to connect the UCC28051 EVM board as the input to a UCC28600 65W EVM for power factor correction (I realize that the rectifier on the UCC28600 65W EVM board will be…
Part Number: UCC28600 I have a UCC28600EVM-65W, I want to reduce the value of Rsu (R2 + R3 + R4) to reduce the start up time. I'm concerned about making the resistance too low, and dropping too much current through the internal zener diode on the Vdd…
Part Number: UCC28600 Hello dear,
I am designing SMSP with power factor correction. The reference design is based on UCC28600 120-W Evaluation board. The power factor correction outputs upto 390V. I am looking for a transformer replacement for the one…
Part Number: UCC28600 Hello dear,
I am designing an AC/DC based on UCC28600, I am uncertain about the input connection of the transformer, that is, Postive and Negative -switching terminal (FA2443-AL - www.mouser.co.uk/.../fa2443-463421.pdf) used in the…