Part Number: UCC28600EVM-65W Other Parts Discussed in Thread: UCC28600 I have an application where the input power into this regulator section will be rectified chopped (phase-cut) AC. The portion of the sinewave coming in may be heavily chopped down,…
Part Number: UCC28600EVM-65W Other Parts Discussed in Thread: UCC28600 , Hello E2E forum,
I currently trying to do simulation of UCC28600 using TINA TI based on UCC28600EVM-65W parameter.
The attached below were my simulation model,
the problem is by using…
Part Number: UCC28600EVM-65W Other Parts Discussed in Thread: UCC28600
Hi,
I want to have 5V 13A from this board mentioned in title what kind of changes should I make? Is it possible not to change transformer and get 5V output?
Thanks and best Regard…
Part Number: UCC28600EVM-65W
Hello TI team,
The question is related to the Q3 on the related questions.
So i intend to using this eval board by populating its OUT2 to achieve different voltage output (for now 5V)
The questions are:
If i populate the…
Part Number: UCC28600EVM-65W Other Parts Discussed in Thread: UCC28600-Q1 , LM4041-N-Q1 , , TL431 Dear team,
Recently my customer wants to evaluate our UCC28600-Q1, and they have three questions as below, could you please help answer them? Thank you!
1.…
Part Number: UCC28600EVM Hi team,
My csutomer is testing new UCC28600EVM-120W, and the following is test results:
1. Efficiency 75% @ 1A; Efficiency 83% @ 3A;
2. 0.5W standby power;
3. No overcurrent protection.
Do you think this is normal result? Please…
Part Number: UCC28600 I have a UCC28600EVM-65W, I want to reduce the value of Rsu (R2 + R3 + R4) to reduce the start up time. I'm concerned about making the resistance too low, and dropping too much current through the internal zener diode on the Vdd…
Part Number: UCC28600EVM
Hello TI Community,
I am trying to accomplish the following: I need a QR flyback controller to take a Vin=48VDC and step it up to an isolated Vout=400VDC at 0.5A output current. I am experimenting with the UCC28600 evaluation…
Part Number: TMS320F28379S Other Parts Discussed in Thread: TIDM-1001 Hi,
In TIDM-1001, the controller's power is fed by UCC28600EVM. I searched and found that there are two EVM, one is called UCC28600EVM-65W , the other one is called UCC28600EVM . which…
Hi,
I am looking for some solutions on designing the SMPS on the below specs, found something from Ti UCC28600EVM-65 but have few questions.
- Input voltage range: 100~240 Vac
- Output voltage: 24V
- Output current: 4A
- Isolated output: Yes
- Efficiency…