Part Number: UCC28630 Other Parts Discussed in Thread: TIDA-00386 , MCF8316A ,
We developed a low voltage ceiling fan controller using all TI devices.
Power Supply : TIDA-00386 Power Supply no changer, Flyback transformer is Wurth 750343068
Motor Control…
Part Number: UCC28630 Other Parts Discussed in Thread: UCC28710 , PMP9041 , UCC28730 Hi,
I want to design a flyback converter topology used power supply that can give me 24V and 2A output from 90V to 265V. I have also seen some designs from TI websites…
Part Number: UCC28630 Other Parts Discussed in Thread: UCC28631 , UCC28704 Hi team,
My customer are currently designing with the UCC28630, but their input supply is going to be coming from a high voltage, DC battery. Due to the input, and lack of AC, do…
Part Number: UCC28630
Hello,
I'm having some issues making our SMPS to start up fully. It seems that it passes the 3 exploratory pulses and starts up and eventually latches up as time progresses.
Please see the schematic, layout and some waveforms…
Part Number: UCC28630 Other Parts Discussed in Thread: UCC28634 , UCC28631 Hi Team,
My customer is considering using UCC28630 to design Dual switch flyback, input 326Vdc~848Vdc, 3 outputs(total100W max): 12V/83W , -12V/3.6W, 5V/2.5W, expect efficiency…
Hello,
I reviewed your schematic and noticed you are not using an RCD clamp. If you are not should try adding one. The application note you have gives instructions for setting this up.
I also notice that you are not using a capacitor on the Vsense pin…
Part Number: UCC28630 Dear Teams,
My customer is looking the UCC28630EVM. They are not able to find the datasheet of L1 inductor (Renco Electronics RLTI-1099/8) from Internet., and I did the same thing while does not works. Could you share the datasheet…
Tim
Best place to see what expected waveforms for UCC28630 is the EVM http://www.ti.com/tool/UCC28630EVM-572 . The user guide for this EVM has typical waveforms http://www.ti.com/lit/ug/sluuax9b/sluuax9b.pdf?ts=1590872018331 . If it does not include a specific…