Part Number: UCC28631 Other Parts Discussed in Thread: UCC28630EVM-572 , , UCC28630 , UCC28632 , UCC28633 Team,
My customer has the following questions:
Is there a soft-start mechanism? (Datasheet says yes but not much info)
How does the soft…
Part Number: UCC28631 Other Parts Discussed in Thread: UCC24650 Hi, team.
Out customer is evaluating a load response test in UCC28631.
In a transient test from zero load, very big drop is observed.
But test from sub mA load, it is improved.
Is…
Part Number: UCC28631 Hi, team.
Our customer designed 15W(12V/1.25A) adaptor using UCC28631.
But very slow output ripple is observed, time period is about 180~200Hz and peak-to-peak ripple voltage is about 200mV
Could you think any reason?
Where…
Part Number: UCC28631 Other Parts Discussed in Thread: UCC28630
Hi, team.
Does UCC28631 have a Over-Power Mode?
Is the Maximum Output Power of UCC28631 100% of Pnom?
Bernard,
I had found and bypassed that long ago by running it off of a separate rectifier.
What I was seeing was the output flying high instead at low frequencies. I did not test to see WHEN it came down but it was at 60mA load so I did not care…
Thank you for your fast response and detailed answer!
Checking the code at the SD pin, it is indeed fault #23. The HV pin is connected to V_Bulk through two series 100k resistors, and the explanation given is consistent with other circuit behaviors…