Part Number: UCC28634 We are designing a high voltage DC-DC flyback converter using the UCC28634 controller. The circuit is currently operational (starts up and somewhat regulates), but is not functioning properly due to excessive ringing on the AUX winding…
Hello Jagadish,
Thank you for your interest in the UCC28634 flyback controller.
For a flyback topology, the transformer symbol in the Altium schematic that you posted has the CORRECT polarities shown for each winding connection. In other words, the…
Hi Murali,
Thanks for reaching out. Yes the calculation tool can be used for 300Vrms input. The excel calculation tool is recommending 2uF/W of nominal output power. If you update cell E12, the recommended input bulk capacitance should update as well…
Part Number: UCC28632 Other Parts Discussed in Thread: UCC28634 I'm trying to use the webench to design a 120VAC to 24VDC power supply. I must have clicked through at least 25 designs at this point, and all of them seem to share the same transformer topology…
Part Number: UCC28633 Other Parts Discussed in Thread: UCC28634 , UCC28631
Dear Sirs. We have designed a flyback conveter using the UCC28633 with a defined output of 65V following the recomendations from corresponding technical notes. But we are having…
Hi Mike,
Thanks for your reply.
Also, customer is considering DC HV start up, can you help clarify the difference between UCC28631 and UCC28634? Thank you!
Regards
Yunjing
Part Number: UCC28631 Other Parts Discussed in Thread: UCC28634 , , UCC24612 , UCC24610 , UCC28630EVM-572 I am currently running a UCC28631 but after a short interruption of the mains, it will not restart until the bulk DC has bled to almost zero or Vcc…
Hi Jayaprakash,
We currently do not support multi-output power supply designs in new WEBENCH power designer tool.
Alternatively, you could design each output separately.
Could you please let us know if application for DC to DC converter is isolated…
Part Number: UCC28630EVM-572 Other Parts Discussed in Thread: UCC28631 , UCC28630 , UCC28634 Dear TI,
I am trying to design a housekeeping power supply for one of our products.
Requirement:
Input: 260 Vdc to 710 Vdc
Output: 12 V @ 1.5 A max. …
Hello Gerald,
PCB layout is an important topic for SMPS and many application notes and datasheets address this issue.
General discussions on SMPS layout:
https://www.ti.com/lit/an/snva021c/snva021c.pdf?ts=1661802120154&ref_url=https%253A%252F%252Fwww…