Part Number: UCC28711EVM-160 Other Parts Discussed in Thread: UCC28704 , PMP11612 , Hi SIR,.
please share us the Altium Designer file of UCC28711EVM-160 and PMP11612 of UCC28704
It`s possible to time to market , thanks
regards,
Philip
Other Parts Discussed in Thread: UCC28711EVM-160 , UCC28710
Hello,
I'm hoping you can please help me with a voltage regulation stability issue I am having. This issue is occurring on both my board and the TI evaluation board that I have, UCC28711EVM…
Hi Mike
Thanks for your recommendation.
But I don't understand why you push UCC28711EVM-160 as the reference design for this case. This design doesn't quite meet the design requirement in this case.Could you explain why you push this ?
Thanks
Best…
Hello,
There was an application note written on how to design with the UCC28700 PSR controller and goes through an off line design 85 to 265V RMS down to 5V 5W regulated output. Including transformer turns ratio, RMS current and primary magnetizing inductance…
Other Parts Discussed in Thread: UCC28711EVM-160 , UCC28711 Hi
My Customer has question.Please cooperate me.
For UCC28711EVM-160,
R4 and C5 are connected in front of VDD. (22.5Ω and 330nF)
Is there a way to determine this constant?
Best Regard
T …
Part Number: UCC28710 Other Parts Discussed in Thread: UCC28722 , UCC28711EVM-160 Hello,
We are working on Universal input SMPS design using PWM controller UCC28710.
We get reference design from Web bench tool for input Ac of 90-460 Volt and out put of…
Part Number: UCC28711 Other Parts Discussed in Thread: TIDA-00173 , , TIDA-00315 , UCC28700 In my new design including the UCC28711 in a flyback power supply, I have some calculation questions:
I checked next documents:
a) TI reference design "400 to 690…
My primary suspect would be the resonance of the primary inductance and the switch node parasitic capacitor. The resonance is typically between 650 kHz and 950 kHz depending on the transformer and FET used (for the UCC28711EVM-160 the primary inductance…
Hello Horst,
Hope you have had success resolving this issue. I am observing the same type of output ripple behavior with my UCC28710 application and was wondering if you could share your outcome?
I find that the UCC28710 is able to operate in regulation…
Other Parts Discussed in Thread: UCC28711 , UCC28710 , PMP8477 , UCC28711EVM-160 , UCC28700 Hi Team,
I have an application where I want to use the UCC28710D to create a 5-V, 2.3-A rail. The UCC28710D doesn't have an EVM, and I have seen the suggestion to…