Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: UCC28780 Hi experts,
I am testing UCC28780EVM-002 with 90Vac(60Hz) input and 45w@20V 2.25A output ,but the power efficiency is much lower than that in EVM user‘s guide. I wonder what cause…
Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: TL431 , UCC28780
Hi Team
UCC28780EVM-002 directly modify the TL431 voltage divider resistor "R24 to 38.3KΩ" will become 12V output, do other parts need to be modified?
Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: UCC28780 Hi Experts, Good day. I need your help. Our customer currently has a UCC28780EVM-002, and they are trying to modify it to their liking, specifically dropping the output voltage from…
Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: UCC28780 Hi,
Good Day. The customer is currently running tests and evaluating the board UCC28780EVM-002.
He is looking to change the duty cycle on the PWML and the PWMH on the controller itself…
Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: UCC28780 Hello E2E Experts,
Good day.
I am currently looking for help with my UCC28780EVM-002. It seems I am getting a fault delay while measuring at Vdd, and am getting 0 V of output instead…
Part Number: UCC28780EVM-002 Hi,
Customer have encountered issue regarding the EVM, please see details below.
I first tried to power it up with 120VAC/60Hz (No Load at Output), but the input AC current suddenly goes very large (~8A according to the AC…
Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: UCC28780 Dear Sir,
I am planning to design a planar transformer, target operating freq was 500khz.
To test this and to know the transformer output voltages. I brought the UCC28780EVM.
Initially…
Part Number: UCC28780EVM-002 Other Parts Discussed in Thread: UCC28780 I'm a student who is studying by purchasing the UCC28780 EVM-002.
I'm studying the design of active flyback converter using UCC28780 by referring to the EVM.
I plan to use another…
Yunsheng:
Yes, we reviewed the file Jaden sent.
The file with .7z extension is for UCC28782EVM-030 board. and its pcb files are indeed online.
BUT.
What we got with us is UCC28780EVM-002,
The only document we can get from the website for this EVM is the…