Part Number: UCC2891 Other Parts Discussed in Thread: UCC2897 , , UCC2894 , UCC2897A , UCC28951 Hello teams,
I would like to design a offline power supply using forward converter topology.
The specifications are as follows
Input voltage: 280V to 330V
Output…
Part Number: UCC2891 hi ,
i need some information about UCC2891.I am using that chip into 500 watts dc to dc application.its able handle 500 watts or not ?
INPUT RANGE=60-84VDC,
INPUT CURRENT=8.3A,
OUTPUT VOLTAGE=14
OUTPUT CURRENT=35A
POWER=500 watts…
Part Number: UCC2891 Other Parts Discussed in Thread: TINA-TI I am using IC UCC2891D need current sharing method
how to use current sharing techniques
please provide detailed design process and understanding PMP2214 PM2214.pdf
Part Number: UCC2891 Other Parts Discussed in Thread: UCC2897A Hello E2E,
I know this device has 13.5V threshold for startup and it stop when the VDD over threshold. However, this characteristic detail is not find on datasheet. Does the 13.5V threshold…
Part Number: UCC2891 Other Parts Discussed in Thread: , , UCC2892 , UCC2893 , UCC2894 Hello!
Can I use your UCC2891X with Secondary-side regulation?
I do not have auxiliary winding and would like to power the IC from the primary winding and use an optocoupler…
Part Number: UCC2891 Other Parts Discussed in Thread: LM5026 , , UCC2897A Hi,
This is Rock.
May I check the UCC2891 or LM5026/UCC2897A can meet the following protection function of SPEC requirement?
Specification Vin: VDC 40~60V Vout: VDC 30V +/- 3% …
Part Number: UCC2891 Hi TI,
I read a post in relation to the magnetizing inductance of the transformer used in the SLUA303 technical note, PA0810, and I still have a doubt, because the transformer manufacturer (Pulse eng) specifies a Lmag=345uH, and a…
Part Number: UCC2891 I have my voltage input from 19.2 to 148v and I want an output of 5v@12A, 15v@3A and -15v@0.5A. I am thinking to make the active clamp forward converter. Will UCC2891 works in this input range? If any reference design available please…
Part Number: UCC2891 Specifications are given in excel calculation sheet
I made this simulation but I am not getting the correct output. I have attached the calculations(made by me) and tina simulation with this. I am getting convergence problem as I…