Part Number: UCC28951 Other Parts Discussed in Thread: LM5046 Hey All,
I'm working on a PSFB converter and wanted to control just the primary RMS current of the transformer, I was wondering if the UCC28951/LM5046 can work with just such an application…
Part Number: UCC28951 Hello,
I am designing a 2.4 kW PSFB DC-DC Converter. I am using UCC28951. I have used the excel tool provided during my power stage design, and I also used the values of the compensation network from there. I have attached the…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951
Tool/software:
Hello Mike,
Two output windings are connected in series. Output is regulated to 26V.
Below waveform is before it enters regulation, voltage is around 300VDC, load…
Part Number: UCC28951 Other Parts Discussed in Thread: UCC28950 Tool/software: Hello,
I am interested in using WEBENCH to design a multiphase UCC28951 regulator. WEBENCH generates designs with UCC28951, but these designs are limited so a single regulator…
Part Number: UCC28951-Q1
Tool/software:
Hello Mike,
Attached is image of output ripple. Is this acceptable? Or it's not ??
Vin : 666 , Iout : 39A, Vout : 25.8V
Purple: output voltage ripple
Below image is for lower loads without…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 Tool/software: 1. Share me data for doing PSFB using SIC mosfets. Presently For next revision schematic I'm referring TOshiba 5KW reference design ( 5 kW Isolated Bidirectional DC-DC Converter…
Part Number: UCC28951 Hi
i am facing a problem with UCC28951 design.
Its a AC to DC converter rating of 58V/40A. When i am loading more than 20A observed some disturbance in mosfet gate wave form. Please suggest what could be the problem.
Attached…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951
Tool/software:
Hello Mike,
I do not understand the reason for closing the previous thread without finishing all queries.
Moving On to the previous reply, I do not follow you…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: UCC28951 Tool/software: Hello,
I am designing a phase shifted full bridge circuit using the TIDA-020031 reference design, with an output voltage of 70V, a current of 45A, and a maximum power…