Part Number: UCC37322 When VDD is 12V what is the recommended way to drive the Enable pin. Do I need a special driver. Can The ENBL pin pull-up be changed? Please provide some examples if available.
Im planning to use UCC37322 and implement this part…
Part Number: UCC37321 Other Parts Discussed in Thread: UCC5390 Dear TI experts,
I want to make 2x ucc37321 being in parallel that is connected directly to eachother pin for pin in order to enlarge the output current , Is that ok ?
Thanks,
John
Part Number: UCC37321 Hi, as the title suggests I'm a bit confused as to what the maximum voltage on the input pin can be. The datasheet states 6v or Vdd (in my case 12v for Vdd) as being the maximum, which one is it?
At the moment I'm currently…
Hi,
Has the request for the model for this UCC37322 been processed?
If not, what other gate driver already available on TINA-TI possibly comes close to this considering its a 9A driver.
Suggestions please.
Thanks
Abdul Nilar
Hello,
It seems the current sense circuit filter (R_filt and C_filt) cannot get rid of the switching noise which could trigger the DRV110 current regulation comparator.
Possible reasons to have a strong switching noise:
1. There is no local ceramic capacitor…
Part Number: UCC37321 Other Parts Discussed in Thread: UCC37322 , around 2 or 3 months ago, I ordered 5 sets of ucc37321 and ucc37322, and around 1 week ago I got the time to use it in a project, but when I powered the project on, the ucc37321 ic keeps…
A list of schematic review templates for many of our devices are available below! These templates are meant to be used in conjunction with our datasheets to help designers review their schematics.
UCC27516 and UCC27517 Schematic Review Template
UCC27511…
Hi Rogers,
Thanks for reaching out on E2E!
Please see the following feedback:
IN: Input looks good. If there is a lot of noise on your input waveforms, consider adding an RC filter with a TC of no greater than 20 ns.
EN: I notice that the label is a NC…