Hi. Been busy with other projects, but had now time to look this again. Where would you mount the X and Y-capacitors? Over the T3 transformer?
I had good results in another project with PI-filter in the input and decided to try it here also after CM-coil…
Part Number: UCC3895
Hi ,
I would like to understand the relation between the EAP Voltage and Phase shift induced by the IC between OUTA and OUTC or OUTB and OUTD.
I would like to use the IC in the voltage mode. EAN and EAOUT are shorted. I will vary…
Part Number: UCC3895 When I try to import the UCC3895 .lib file (provided on its page on the TI website), I get this error:
Is there any way of modifying (or un-encrypting) this file for use in TI's own program?
Part Number: UCC3895 Hi expert,
Customer designed with UCC3895 in ~14kHz Fsw. With RT=100kohm and CT=6.8nF which is far more than CT recommended max value 880pF.
What's the risk for doing this with high CT? The discharging current may be high and do…
Part Number: UCC3895 Other Parts Discussed in Thread: PMP9622 Hi team i got some questions about the pmp9622 question 1 is the R35 tied to ground( 0V ) or tied to 5V supply. as the figure below. question 2 why is the r28 supplied from 6.3V is there a reason…
Part Number: UCC3895 Other Parts Discussed in Thread: TL081 , PMP9622 , PMP8740 Hello,
I am using UCC3895 in a Full bridge converter 48V DC input, 320V DC output. I want to insert a current regulator on the output with a shunt placed in series on the +320V…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC2895 , UCC28950 Hi TI team,
Whether UCC3895- Phase shift controller IC can be used for Isolated DC-DC Converter for 500W design, can we use the same IC for secondary side synchronous rectification…
Part Number: UCC3895 hi,
i am using uc3895 controller for my dc-to-dc converter application this is full bridge topology, but we need half bridge, suppose i will use only two signal from input QA, QB) its anything problem?
because of my input voltage…