Part Number: UCD3138 Tool/software: One of our mass-produced products using the UCD3138 experienced a problem with the PWM waveform not expanding properly during customer application, resulting in abnormal output voltage. After receiving the module in…
Part Number: UCD3138 Tool/software: HI.
My hardware designer has put 2 UCD3138 on the same PMBUS.
I am in charge of the firmware design.
According to docs, in Romcode, @ for PMBUS is set at <0xB>
How can I flash the UCD when they are empty…
Part Number: UCD3138 Other Parts Discussed in Thread: UCD7138 , Tool/software: Hi,
Just have seen this topic and I have some questions: UCD3138: Multiple Interleaved Dual Active Bridge Converters with Phase Shedding
I need to control four different…
Part Number: UCD3138 Note: This is a resubmittal of my information request (case #CS3304970) to the E2E forum.
------------------------------------------------------------------------------------------------------
Hello,
I have an RF amplifier application…
Part Number: UCD3138 Tool/software: Hi E2E,
Please help to check the following question, thanks,
Normal operation (upper left picture): When MCU_VDD 3.3V is established, it is judged that V_Bulk > 390V, PFC_OK transitions (from HI to LO), and the…
Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138 , , USB-TO-GPIO2 I used ucd3138 as the main control chip for the bridgeless totem-pole PFC power supply. After manually running the code using the Device GUI, the bridgeless totem-pole PFC…
Part Number: UCD3138 Other Parts Discussed in Thread: PMP21529
I set the board into the ROM Mode
Then I connected the board via XDS100V2 the target is not working
Error Log,
[Start: Texas Instruments XDS100v2 USB Debug Probe_0]
Execute the…
Part Number: UCD3138 Other Parts Discussed in Thread: , PMP20873 Tool/software: 1. May I ask if there are any relevant documents about the code that I can learn?
2.In the code, is there an implementation of the documented content? How to reduce current…
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138128 , UCD3138 Tool/software: Hi,
The CIM on UCD3138A does not have the mask for UART0, only UART1 and 2
Is the UART0 using a different interrupt handler? And how do I figure it? It will…
Part Number: UCD3138 Tool/software: Hi expert,
My customer would like to adjust the UVP setting of UCD3138RJA. Can you please comment how to adjust the UVP setting thru the PMBus?
Best regards,
Randy