Part Number: UCD3138ALLCEVM150 Other Parts Discussed in Thread: UCD3138ACCEVM149 , , UCD3138A , USB-TO-GPIO2 , UCD3138 Hi Team,
I am trying to use the UCD3138ALLCEVM150 evaluation module. As a part of that I gave 12V external supply (through J1) to board…
Part Number: UCD3138ALLCEVM150 Hi TI Experts,
UCD3138ALLCEVM150
www.ti.com/.../UCD3138ALLCEVM150
For this EVM,
(a ) Does this EVM have GUI setting tool ?
(b) Does this EVM have UART Interface to send debug message out?
(c) Does this EVM have UART Interface…
Part Number: UCD3138ALLCEVM150 Other Parts Discussed in Thread: UCD3138 , Hi TI Experts,
We use EVM "UCD3138ALLCEVM150" and software "UCD3138FW_LLC(UCD3138 LLC Half Bridge Firmware)". The default voltage output is 12V. If we want to modify…
Part Number: UCD3138ALLCEVM150 Hello experts, I am currently using UCD3138ALLCEVM-150. I have downloaded TI's official routine, but it is a closed loop program. If I want to change it to an open loop program first, where should I start? This closed loop…
Part Number: UCD3138ALLCEVM150 When I use a DPWM2 module and a comparator D to trigger a period-by-period current fault:
The setting of DPWM2 is:
In the open loop state, set the mode to normal mode, period value, and event 1, 2, 3, and 4 values to 10000…
Part Number: UCD3138ALLCEVM150 Other Parts Discussed in Thread: UCD3138A
When I conducted DPWM high-resolution testing on the control board UCD3138ALLCEVM149, I found the following abnormal situations
The test conditions are:
UCD149ALLCEVM3138…
Part Number: UCD3138ALLCEVM150 Hi,
I have a UCD3138ALLCEVM150 control board.
Can you please specify the resonant frequency of the LLC converter?
If possible, kindly share value of external resonant inductance (L1).
Also, I will be grateful if the transformer…
Part Number: UCD3138ALLCEVM150 When I use a DPWM2 module and a comparator D to trigger a period-by-period current fault:
The setting of DPWM2 is:
In the open loop state, set the mode to normal mode, period value, and event 1, 2, 3, and 4 values to 10000…
Part Number: UCD3138PFCEVM-026 Other Parts Discussed in Thread: UCD3138ALLCEVM150 Hi TI Experts,
UCD3138PFCEVM-026 has a UART (uart1)to communicate with secondary. If I use UCD3138PFCEVM-026 (PFC) and UCD3138ALLCEVM150 (LLC) as Primary and Secondary, is…