Part Number: UCD3138FW-PSFB Hello:
The LLC expert refers me to ask the following question to PSFB experts. So here you go.
Fortunately for us, the modified LLC breadboard by putting in our values just to ensure we get a better understanding of the circuit…
Part Number: UCD3138FW-PSFB Other Parts Discussed in Thread: UCD3138
Hello
I imitated the PSFB development board of UCD3138 to make a power supply prototype,
and encountered a problem when doing load jumps.
When the load jump amplitude is small, such…
Part Number: UCD3138FW-PSFB Other Parts Discussed in Thread: UCD3138 Hello,
I imitated the PSFB development board of UCD3138 and made a power supply,
and found that when the loop bandwidth is 6kHz, Vo will oscillate obviously when the load jumps from 0A…
Part Number: UCD3138FW-PSFB Hello
I recently tested UCD3138-PSFB EVM and found two problems:
1. When the development board is unloaded and slightly loaded, the phase shift angle of the primary switch tube is very different. When there is no load, the…
Part Number: UCD3138FW-PSFB Other Parts Discussed in Thread: UCD3138 Hello
I imitated the PSFB development board of UCD3138 and made a power supply
During the test, it was found that the output voltage was the target value when the prototype had a load…
Part Number: UCD3138FW-PSFB Hello, I made a power supply modeled on the PSFB development board.
When debugging the load jump from 6A to 10A, the synchronous rectifier is damaged, the waveform is as follows:
The green curve is the output current, and…
Part Number: UCD3138FW-PSFB
Hello, may I ask why UCD3138PSFBEVM-027 software code shield this sentence, if the system locks, how to do? Looking forward to your reply, thank you!
Part Number: UCD3138FW-PSFB Hello, the DAC_SEL of the front-end 2 in the "UCD3138FW-PSFB" software code has been set up many times, but none of them uses EXT_DAC2_EN=1, so how can DAC_SEL work? I feel that some of the annotations in the software configuration…
Part Number: UCD3138FW-PSFB Hello! There is a question about the voltage loop configuration in CPCC mode. As shown in the figure, will the CPCC module not automatically set the given value of the voltage loop? Do I need software to calculate voltage settings…
Part Number: UCD3138FW-PSFB
Hello, what is the register LoopMuxRegs. CPCTRL. bit. THRESH_SEL used for in CPCC mode? Looking forward to your reply, thank you!