We do not support programming through the Linux operating system.
Attached find the document Configuration Programming of UCD Devices.
This contains several methods for loading the configuration into a UCD Device.
PMBus scripting method may be what…
Exercising nRESET shouldn't cause any problems but there should be no need to use it during normal operation (power conversion) of the device. As for programming, the PMBus script that can be exported from the Fusion Digital Power Designer contains all…
Hi Phillip,
What configuration file format do you generate for JTAG programming? If you use File->Export... to generate SVF or HEX files, the PC needs to connect to an online device to generate the files. This is because the SVF and HEX files are images…
Hi Dave,
TSW14J58EVM Rev C will be powered using 12V. TP1 is connected directly to the input jack as well. Please find schematic below.
TSW14J58_RevC_Schematic.pdf
Regards, Chase
Thank you, Jim, for your support. I found the schematic for the JESD204B Translation Card in one of your previous posts ( /cfs-file/__key/communityserver-discussions-components-files/73/2337.JESD204B_5F00_TRANSLATION_5F00_MIXED_5F00_C_2D00_SCH.pdf ) …
The Fusion Digital Power Designer uses the USB-to-GPIO to communicate with the sequencer.
Refer to the following document for information about configuration loading.
0652.Configuration Programming of UCD Devices.pdf
Hi Frantisek,
In programming aspect, UCD90160A is same as UCD90160.
Please see attached document. 8726.Configuration Programming of UCD Devices.pdf
Regards,
Zhiyuan
There can be several ways to program the device. In general, the steps are: (1) Find out which method the programmer uses to program the device, (2) Use Fusion Digital Power Designer GUI to export the file corresponding to the programming method, (3)…