Hi Anne,
Got it, I can understand what's your expressing in previous captions.
I think that it's okay for user to further check fault logs in sequence with 0xEBh and 0xECh, not just using 0xEAh to check for all fault logs.
That's would be helpful…
Hi Yihe,
Got it, I have seen that chapter about FW programming caption and example.
Do you have any sample code about UCD90160A sequencer FW (hex data format) online update into memory for reference?
Thanks a lot.
Best Regards,
Paul Lei
Part Number: UCD90160A Hi,
Which hardware do I need to use to program the UCD90160A via JTAG?
Is there any USB blaster connecting to the TI GUI?
Another question -
Does the TRSTn pin is an optional pin for device programming or is it mandatory?
Thanks…
Part Number: UCD90160A Hi TI e2e team,
I have one question about UCD90160ARGCR hardware design change, could I change capacitor from 1uF (CAP_SMT_0603_1UF_16V_+/-10%_X6S) to 2.2uF (CAP_SMT_0603_2.2UF_10V_+/-10%_X7R) at C484 location for BPCAP pin in below…
Part Number: UCD90160A
Hi,
When I put in the enable names for the all the 16 rails and save the config file the enable names are not being saved in the config file for some reason. When I reopen the config file that I saved the enable pin names are gone…
Part Number: UCD90160A Hi,
In my case, i am using MON1 pin used for the 3.3V monitoring Purpose, in GUI, as a fault response, if Under voltage or Over Voltage fault is happened, we are disabling all other rails by making enable pin low.
so 3.3V fault happened…
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90120A How can we enable current monitor function for UCD90160A in the Fusion Digital Power GUI? Looks like UCD90120A is okay to monitor current but UCD90160A is not supported yet. Why not add curent…
Part Number: UCD90160 Hello expert,
My customer would like to know UCD90160 code can program UCD90160A or not. I checked with previous reply from Yihe, hex file cannot program A version and xml can program A version. But my customer is using hex file…
Part Number: UCD90160A Hi TI service team,
Could you help to review attached SCH file for "UCD90160ARGCR" HW design check ?
Please help to regard all parts as stuffed components in design.
Thanks.
TI_UCD90160A_SCH_CHECK_V1.0_20231106 (with WM…