Part Number: UCD90320EVM-783 Hello,
In the document SLVA845A - Design Voltage Margining Circuit for UCD90xxx Power Sequencer and System Manager it says that ideally R3 and R4 for the voltage margining circuit should be equal.
This is reiterated in th…
Part Number: UCD90320EVM-783 Other Parts Discussed in Thread: UCD90320 You previously suggested for the below circuit that: "The Vout Scale Mon has to be set to equal to scaling ratio in your schematics. For your case, the ratio is 2.49/12.49 = 0.1994…
Part Number: UCD90320EVM-783 Other Parts Discussed in Thread: UCD90320
Hi,
I want to monitor 12V and I have used following voltage divider. VCC12_MON goes to AMON pins.
What value should I have to set in Vout Scale Mon field of Fusion GUI.
Part Number: UCD90320EVM-783 Hi,
Can we configure a voltage rail without any enable pin to it.
Ex: I have voltage rail to monitor say X. It is being derived (through some coupling) from some other voltage say Y rail which is also I'm monitoring.
…
Part Number: UCD90320EVM-783 Hi,
I'm programming UCD90320EVM-783. Now I want to export the config file which I have saved in .tifsm format.
I'm not getting the export option.I'm programming in the offline mode.
Your document shows File>export…
Part Number: UCD90320EVM-783 Other Parts Discussed in Thread: UCD90320 Hi,
I have few doubts related to Powering-ON the UCD90320EVM-783.
Q1. If 5V DC input is connected and jumper J24 is shorted, then is it possible to connect HPA172 to the FRC-10 pin…
Part Number: UCD90320EVM-783
Hi,
I want to know how a command controlled GPOs are controlled through PMBus commands and through Fusion software.??
I have created a Command controlled GPO in Fusion software (say X), then how to toggle 'X' through PMBus…
In order to configrue a commanded based GPIO.
the followiing commands are need in a pari:
1. GPIO_SELECT(0xFA). this command is to select which pin to configure. The value used with command is the Pin ID(pin index) defined in the table 11 http://www.ti…
Hi
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/901014/ucd90320evm-783-adc-input-resistance-for-the-ucd90320/3330964#3330964
Regards
Yihe
Part Number: UCD90320EVM-783 It appears from the BOM and the pictures that are shown that the IC is populated on the EVM board.
I cannot truly tell from the layout files shown, but could a socket be installed so that the customer could use this device…