Part Number: UCD90320 Hi Team,
Per the datasheet, the “U” suffix part is recommended for “Telecom and Networking” equipment. In addition, they reference SEU events
Features
Ultra Low Alpha(ULA) Mold Compound to reduce soft errors…
Part Number: UCD90320U Other Parts Discussed in Thread: UCD90320 , Hello,
We already program the flash memory of UCD90320 using I2C-PMBUS commands. Is there any difference between flash memory programming of UCD90320U and UCD90320? What is the flash memory…
Part Number: UCD90320U Other Parts Discussed in Thread: UCD90320 ,
Could I use UCD90320 configuration file (.cvs / .xml / .tifsp) on UCD90320U ? If yes, how?
I have tried the follow method:
1) Create new offline system from start --> select UCD90320U -…
Part Number: UCD90320U Other Parts Discussed in Thread: UCD90320 To whom it may concern,
Is it possible to have a copy of the binary for the UCD90320U firmware. I have the follow communication error. Can re-flashing the firmware work?
Part Number: UCD90320U Other Parts Discussed in Thread: UCD90320 , Hi there
I have two image files (.XML and .tisfp) was built based UCD90320U. However the we want to program to UCD9032. It seems the image files can not be programmed to UCD90320.
How do…
Part Number: UCD90320U Other Parts Discussed in Thread: INA190 , I have a UCD90320U which is set up with multiple MON pins as current monitors. I am using the INA190A5 current sense amplifier and a variety of shunt resistor sizes. There are no additional…
Part Number: UCD90320U Hi there
If LGPO's polarity is set to active high with actively driven, does it mean output is low when the logic input NOT true?
Thanks
Mike
Part Number: UCD90320U The polarity is active high when logic result is true, does it mean the output is low when the logic input is NOT true?
And Vise versa
Thanks
Mike
Part Number: UCD90320U Other Parts Discussed in Thread: UCD9090A ,
Hi there
1. I want to set MAR2 pin as a GPI pin in Fusion Design tool . How to do that?
2. How do I add MAR5 as GPI function in Fusion Design tool?
Thanks
Mike