Hi
I would recommend on this quick guide
5756.UCD90xxx 简易使用手冊.pptx
most rail has control pin as ON/OFF_CONFIG. so you have to ensure that the pmbus-control pin is at right state to turn on rail
Regards
Yihe
Hi
do you mean GPIO instead of GPIP?
Based on what you list, I do not see why you need PIN SELECTED RAIL STATE?
Please take a look this.
1715.UCD90xxx Quick Guide.pptx
Regards
Yihe
Hi
I try to understand here.
You want to connect the MONx of UCD90 to the output of the power supply controlled by another power sequencer and let the UCD to check whether the output comes up in a right way
Or you want to connect the GPIO of UCD90…
HI
If the output is reverted, it means that the conditions are not met to output correct signal.
Please check your configuration file.
This attachment may help you to understand how the part works.
Regards
Yihe 5460.UCD90xxx Quick Guide.ppt…
Hi
Once rail is on, on dependencies change won't impact it.
off dependencies won't trigger a off since it is a conditions only.
Please refer this guide to understand more
3362.UCD90xxx 简易使用手冊.pptx
Regards
Yihe
Hi
Please refer this quick to understand for the sequencing.
53380.UCD90xxx Quick Guide.pptx
For the margining and monitoring, the margining will not start until the followings are met:
1. the rail reaches its POWER_GOOD threshold
2. customer…
Hi
Yes, when the rails' ON/OFF_CONFIG is set to AUTO(none). the rails can not be shutdown unless either of the following occurs:
1. the rail has fault and the fault response is set to shutdown.
2. UCD has lost its onw powers.
Please refer the…