Hi,
We perform systematically an construction analysis of bought components. We have recently bought UCD9220 and UCD9090: these 2 references contained a die (chip) having the die marking "UCD9240". Is it normal?
Regards,
Denis
Part Number: FUSION_DIGITAL_POWER_DESIGNER Hi ,
I saw from description FUSION DIGITAL POWER DESIGNER support for UCD9220 — 2MHz, 2 rail, 4 phase digital PWM buck controller.
Could help me to check the FUSION DIGITAL POWER DESIGNER GUI support for…
Hi Qammar,
Is there a reason why you needed to mux the TSENSE signal from U39 (PTD08D210W) going into the UCD9248. There is an example schematic of a typical dual output application shown in Figure 22 . The typical schematic shows the TSENSE lines going…
Part Number: UCD9248 Other Parts Discussed in Thread: PTD08D210W Dear UCD9248 team:
I tried to reprogram UCD9248 with Manufacturing Tool back to factory defaults for VC707 boards.
But the GUI always stuck at the 'validating' and failed. Please see the…
Yes, I believe so, but just in case, see the attached. I downloaded the tools earlier this week, so I expect they are current. I am using version 7.4.1 of the Fusion Digital Power Designer to make the changes. I have also used it in the offline mode…
Other Parts Discussed in Thread: UCD7231 , UCD9220 Question1 :
I had reflect of UCD7231 application circuit which possible of boost convertor from reverse think of buck convertor circuit .
I mean If when I think that exchange to input and output, Is It applicable…
Part Number: UCD9246 HI,
I am doing some testing on UCD9246 based power supply. When I chnage the switching frequency in GUI, the GUI is crashing and showing Fatal Error. I tried to change the frequency when all rails are in OFF condition. Is there any…
Yes, both the UCD9220 and UCD9240 datasheets are incorrect in the specification of the t(timeout) as 35us max, you are correct that it should be 35ms.
I will have this added to the errata sheet for these devices, the newer controllers have already been…
Unfortunately we do not have a UCD9240 EVM. You could use the UCD9224EVM. It will give you a good idea how these parts work. The UCD9220 has two outputs and up to four phases versus the 4 outputs and 8 phases of the UCD9240.
Other Parts Discussed in Thread: UCD9244 , UCD9220 For the UCD9244, what should i do with any unused input pins? Specifically, I'm wondering about unused VID pins, unused inputs to the 12-bit ADC (CS, temp/aux, etc) and unused inputs to power peripherals…