Part Number: TPS25751EVM We are using TPS25751EVM and programming it by USBCPD ACT. We would like to have some interrupt to inform other components, so we assigned an event to GPIO0.
We assigned event #1 PlugEvent_Port1 to GPIO0 for getting the device attached…
Hi Neehar,
Yes I am using J721S2 EVM.
Neehar Sawant said: For examples of toggling the LEDs, you can refer to older SDKs such as 8.6.
Where can I find the older SDK releases?
Neehar Sawant said: Do you solely wish to control the USER LEDs on the GPIO Expander…
Part Number: USB-TO-GPIO2
Hello Team,
In earlier post few years ago Jim Slupe already posted a thread( USB Interface Adapter (SMBus ) about Process Call section. Eventually I'm also facing the same issue. If I enter 0x7D01 for the data payload, it returns…
Part Number: TMS320F28388S Hello Team,
Is it possible to utilize ADC pins in an MCU as digital input pins?
If it's feasible, what additional considerations do I need to focus on when using ADC pins as digital input pins?
Hello Sudhir, Can you please read the GPIOs and confirm they are in the correct state?
Above is an image of the GPIOs and what they are used for. Please be sure that they are not set to the wrong setting.
Best,
Quentin
Part Number: AM6441 Hi, Expert
Customer want to achieve this flow, please help to evaluate feasibility, Thanks.
GPIO as interrupt trigger
GPIO falling edge, interrupt routed to DMA
DMA access NAND via GPMC, move data from NAND to other memory.
Rega…
Part Number: PMP4451 Hi, This board has a J1 Micro-USB type B connector for power input to the board, I want to modify this to replace this with USB-Type C for power input to board. How can I modify this circuit to exchange these connectors. What are…
Part Number: UCD90160A Hello,
Is it possible to use USB-TO-ANY instead of USB-TO-GPIO to programm UCD90160A with Fusion Digital Power Design?
Thank you.
Best regards,
Kübra
Part Number: CC1310 Brief:
I am using CC1310F64 microcontroller in my project with below setup,
rf unit is being used,
there are two gpio pins being used as input with interrupt mode with rise/fall edge detection,
uart with 115200 baudarate
problem: …
Part Number: BQ78PL11XAPI-SW Other Parts Discussed in Thread: BQWIZARD
Hello,
I am currently facing an issue using the bq78pl11x API. Specifically, the bq78pl11x API demo does not recognize or find the USB to GPIO adapter when attempting to discover the…