Part Number: WL1807MOD We are using WL1807MOD with Linux 5.4 on i.MX6 platform. I know that only 4.19 is supported, but I'd like to report our findings anyway. These are the patches we are using:
0002-wlcore-mesh-Add-support-for-RX-Boradcast-Key.p…
Part Number: WILINK-SW Tool/software: Linux Hi Guys,
i have use
above guide for backporting, it has backported perfectly i'm able to get wifi working.
I have created hostapd.conf and udhcpd.conf, with change i reuired,
So far i was using stationary…
Part Number: WL1835MOD Hi Champs,
My customer is testing the WL1835MOD at fixed frequency. The RTTT SW automatically exits after upgrading the FW.
Also when connected to the Wilink module, it shows no MAC and PHY FW version as in the picture.
Please advise…
Hi Welson,
Take AM625 processor for example, the EVM we built named SK-AM62 has used WL1837MOD module, and have the code support.
https://www.ti.com/tool/SK-AM62#design-files
Dual-band Wi-Fi®, Bluetooth®/Bluetooth Low Energy 5.1 via WiLink 8 WL1837MOD…
Hi Albgarc,
1 - You will setup the device to not enable the ANT2 connection
2. Yes, and configure the SW
3 - You'll want to keep half a wavelength away from other signals.
4 - Yes, you could do that as the modules are pin to pin compatible.
5 - You…
Part Number: WL1837MOD
Team,
The getting started guide has been updated and point to the latest Wifi (R8.8) and BT SW: https://www.ti.com/wireless-connectivity/wi-fi/overview.html#gettingstarted See page 3 section 3 of : WiLink 8 Getting started guide…
Hi Hanna,
1. Yes we have various SW packages depending on what host you are using (e.g. Linux processor or MCU).
2. We have 3 products families that support BT (e.g. WiLink, CC25xx and CC26xx) none of them have an internal DAC. May I ask what you need…
Part Number: SIMPLELINK-CC32XX-SDK Other Parts Discussed in Thread: CC3135 Hi Team,
Do we have any direct SW or library functions in our CC32xx-SDK to use the CC32xx, similarly as WiLink, like an gateway to SDIO or SPI w. Interrupt?
Thanks in advance! …
Hi Aasrith,
If you are using the Sitara EMV (AM335) then you need to run this with calibrator commands. Calibrator commands can be found here: https://processors.wiki.ti.com/index.php/WL18xx . From this you can go to the calibration and Testing section…
Hi Daniel,
Are you doing these measurements conducted or Radiated? For a baseline these test should be done conduced. Also when doing this test you need to have attenuation between the DUT and the CMW500 so that the test equipment is not driving a low…