Part Number: WL1807MOD Hi all,
my customer is adopting WL1807MOD as client, and looking to expand to countries where the usage for 5GHz bandwidth is limited.
Should the customer take any action, even if using only as client? Below is the customer…
Part Number: WL1807MOD Hi Experts,
We are using WL1807MOD+WiLink8 in development.
During active scan,
Is it possible to set the frequency to 11g frequency range only?(2.142GHz~2.472GHz).
Also, is it possible to set the frequency to 11a frequency…
Part Number: WL1807MOD I am trying to integrate a WL1807MOD module with a Freescale K66 series MCU. We are in the process of trying to integrate a third party stack for wifi functionality into this. We are running MQX operating system on the MCU. Can…
Part Number: WL1807MOD
We were looking through the WL1807MOD documentation, such as processors.wiki.ti.com/.../WL18xx , still not sure: can we use it with some third party MCUs, such as STM32F? Is there an API over SDIO, SDMMC etc to access its features…
Part Number: WL1807MOD Hi,
According to the datasheet:
In 2.4GHz MIMO I can get 2 20MHz channels from each antenna/RF port for 80Mbps high throughput, but it this means that the 2 channels are contiguous or they are separated by a 20Mhz space? …
Part Number: WL1807MOD Tool/software: Linux Hi Champs,
We still have similar thread discussion.
*If Wireleass communication is over 2km, data disconnected. However dBM value doesn't have any issue.
*If customer use wilink for station and another…
Part Number: WL1807MOD hi,
we are interested in the option of creating system update software in the bootloader stage (using U-Boot on our device).
since wireless connectivity is not supported in uboot (no 802.11 stack)
what will be necessary to…
Part Number: WL1807MOD Hi experts!
My customer is looking at the WL1807MOD for their system and have the following questions. Can you help with this?
We are looking at using the WL1807MOD for a special application. Specifically, we want to leverage…