Part Number: WL18XX-BT-SP Other Parts Discussed in Thread: WL1837 , AM5708 Tool/software: Linux Hi,
We are using ti's wl1837 module for wifi/bluetooth with am5708 processor.
Now, we want to do RF testing for bluetooth in both continuous transmit…
Part Number: WL18XX-BT-SP Other Parts Discussed in Thread: AM5708 Tool/software: Linux Hi,
I'm using bluetooth module Wl18xx with TI firmware from Bluez 5.43 on my board TI AM5708 (Linux kernel 4.4.41).
I'm initializing bluetooth with following command…
Part Number: WL18XX-BT-SP
Tool/software: Linux
Hi All,
We are using the jorjin WG7831-DO module based on Ti Wilink8 WL18XX in our project with iMX6ull based customized board running on Linux Kernel 4.1.15.
I am trying to test the bluetooth interface…
Part Number: WL18XX-BT-SP I'm using BT firmware patch SP 4.2 on WL18xx chip. I have an issue when sending last part of BT firmware patch script during my BT init.
The last part of my firmware patch script looks like this
const unsigned char wl18xx_abPacketBT299…
Part Number: WL18XX-BT-SP Tool/software: Linux Hi Guys,
I'm using wilink 8 wifi chipset in custom DM385 board.
kernel - 2.6.37
I have followed
wilink 8 will be in Access point mode. I'm able to connect most mobile phone to my board. but some…
Part Number: WL18XX-BT-SP Hello,
I am looking to buy a WiLink module for usage with Jacinto 6 EVM revision G running Android for Wi-Fi access. I have been using the module listed in this link . But it is listed as no longer available on the website…
Part Number: WL18XX-BT-SP Is it possible to configure the WL18xx module in a state where it is still listening for devices while the MCU is in a sleeping mode, and it then signals the MCU to wake up when some activity is detected ?
And if it is possible…
Part Number: WL18XX-BT-SP During the execution of build_wl18xx.sh init i get following error message
Setting toolchain --2017-09-20 14:06:32-- releases.linaro.org/.../gcc-linaro-4.9-2015.05-x86_64_arm-linux-gnueabihf.tar.xz Resolving releases.linaro…
Hi Bhavani,
We are targeting the end of this week for the Linux Bluetopia stack. Some internal processes delayed our release.
Thanks for your patience,
Jacob
Hi,
Your query has been assigned to a relevant expert. We will get back to you shortly.
Best regards,
Vihang
Note: The issue above is not related to the WL18XX-BT-SP. Just wanted to mention it to avoid any future confusion.