Part Number: XTCIEVMK2LX Hello
e2e.ti.com/.../604106
Acrding to this entry; Do we have to update RFSDK2_02.00.07.00-src.tar.gz with files which you gave DEMO2_noTx for running DEMO2 properly ?
I cannot make radio on
I get the same error with Huioon Kim
Traceback…
Part Number: XTCIEVMK2LX Hello,
We are using K2L SOC in one of our project. The USIM interface is not working in our. Is there any converter (design / circuit) to convert USIM interface to I2C or SPI or UART signals.
Regards,
Sumathi
Part Number: XTCIEVMK2LX Hello, experts.
I have XTCIEVMK2LX and ADC14X250EVM, and wanna get some data from the ADC and process it on the DSP cores of the EVMK2L. I connected the ADC board with the EVMK2L directly via the FMC1 connector without a DLC board…
Part Number: XTCIEVMK2LX Tool/software: TI-RTOS hi,
i was working on FFTC Example Projects in SDK 3.01.03.06 with CCSv6 (6.1.0.00104 ), Now i migrated to Processor SDK 4.03.00.05 with CCSv7 (7.4.0.00015 ),
( installed "ti-processor-sdk-rtos-k2hk-evm-04…
Part Number: XTCIEVMK2LX Hello, experts.
I'm struggling for getting data from an 3rd party ADC board with XTCIEVMK2LX (see this ). Now I'm considering another approach: using an ADC EVM from TI such as ADC34J22EVM.
So, can I directly connect the…
Part Number: XTCIEVMK2LX Tool/software: TI-RTOS Hello,
I have been working on my own project using the FFT Co-Processor and have been using the "fftcMCK2LC66BiosExampleProject" that shipped in the PDK with Processor SDK 4.0. Since I would like to run…
Part Number: XTCIEVMK2LX Hi
I am using XTCIEVMK2LX...bmc in this evm is implemented in stellaris lm32sd93....
I am able to update bmc firmware using bootloader uart0 port....
I am using ccs 5.1 environment....
I was trying to get access to bmc uC via…
Part Number: TCI6630K2L Hello, I have a customer who is interested in developing LTE base station. According to TI website, TCI6630K2L is suitable for this purpose and EVM seems available. TCI6630K2L: http://www.ti.com/product/TCI6630K2L/descriptio…
Part Number: XTCIEVMK2LX Hi all,
I was using an oscilloscope probe on the AMC connector of my board to see an output signal, and I touched both a ground pin and a 12 V pin.
The board looks (and smells) fried. A red LED (D6 or D7) lit up, the fan stopped…
Part Number: XTCIEVMK2LX Hello, experts.
I'm testing FFTLIB these days and trying to FFT over very large number of points data, 20M-point, with 1D SP FFT R2C kernel (fft_sp_1d_r2c.c).
I utilized the example project of the kernel to write test code…