Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 , TIDA-01536 Hello everyone, I'm using the XTR111 to convert a 0-5V input voltage to a 4-20mA output, as shown in the picture below.
I would like to know in this case the transfer function…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: TIDA-01471 , , XTR111
---------------------------------------------------------------------------------------------------------------------------------------------------------------------------…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 , I am building a V to I converter using XTR111 and need to look at the GERBER files for the XTR111 EVM board to match exactly the traces
I would use just a part of the board where the XTR111…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111
circuit requirements that ı need
VSP:16-40V input voltage range 0-5V output current range 0-20mA Output maximum load resistance: 600ohm
SI3459BDV-T1-GE3
( https://www.digikey.com/en/products…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 Hi Team, Our customer would like to confirm there is a protection of output current IOUT when shorted to VSP or GND? If not, do we have a recommended additional circuit to be added to protect…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 Sir,
many thanks for the simulation of the XTR111 scheme ,
kindly let me know how to use the TINA tool for simulation
so that I can get the correct values
regards
K, Ganapathy
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 Dear Sir,
Many thanks for the suggestion, I could use the TINA simulator and changed some values of the schematic
please see the attached the changes are R 10 = 90 k, V1= 3V (as this is internally…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 Dear Sir, I wanted to use your XTR111 current converter IC to get 4 to 20mA output with an input of 0.5 to 4.5 volts
Based on the data sheet and XTR111 evlauation user maual I have arrived …
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 Hi there,
I am using this Evaluation board as a standard source, as a reference for my 4-20mA.
.
When I use a scope to check the value, look like it is not stable. Can the peak to peak be…
Part Number: XTR111-2EVM Other Parts Discussed in Thread: XTR111 , TIPD102 Hi,
I am designing a circuit for my application which is as described below
I/p: 0 to 10V
I/P step voltage: 10mV
O/P current: 0 to 1024uA
Compliance voltage: 12V
If I changed the…