Part Number: XTR116 Regarding output Vref
spec sheet describes parameters (under test condition column) where Iref = 0 to 2.5mA
I wish to source current up to 3.8mA to increase my bridge circuit sensitivity.
is this recommend ed and what are my limitations…
Part Number: XTR116 Other Parts Discussed in Thread: TPS54062 , XTR111 My circuit diagram shows a 4-20mA transmitter with the XTR116 and TPS54062. Instead of 4mA I get 34mA.What could be the reason for this?
Part Number: XTR116 Other Parts Discussed in Thread: XTR300 Hello,
I want to integrate three 2-wire transmitters, each with its corresponding DAC and digital isolator, and connect the isolator to an MCU via an interface bus.
Question: Can I share the…
Part Number: XTR116 How will this component do if someone shorts the 24v wire with the current return wire, during operation? Will the component be damaged? And lets say that the reference design has been implemented.
Will there be damage to the device…
Hi Robert,
Robert de Boer said: Here is something I found, must replace AFE with processsor to detect, scale and output. Robert de Boer said: Please let me know if you have a microprocessor that fits these requirements.
Please submit an inquiry to our MSP…
Part Number: XTR116 Hi,
As I looked through the latest datasheet of XTR116 (SBOS124B – JANUARY 2000 – REVISED JUNE 2023) , the minimum operating temperature has been changed from -55C to -40C. I'm pleased to know if the construction of the IC has been…
Part Number: XTR116 Other Parts Discussed in Thread: MIKROELEKTRONIKA Hi
I recently purchased a MikroElektronika 4-20mA T Click MCU Add On Board MIKROE-1296 for an application that I need for a project at work, which has a 24V source connected to the…
Part Number: XTR116 Other Parts Discussed in Thread: TLV9052 , OPA391 , OPA187 , TLV2186 , OPA2187 , OPA2186 , OPA192 , XTR105 , OPA186 Are there any recommended circuit modifications we could make when using the XTR116U part that would allow the chip to go into…
Part Number: XTR116 Other Parts Discussed in Thread: ISO7310-Q1
Hello,
We are trying to develop a 4 – 20mA current transmitter. The control is done by a PWM signal issued by a microcontroller.
I can't quite understand the values of R3 (Rin) and…
Part Number: XTR116 Other Parts Discussed in Thread: ISO7321FC Hi Team,
According to our customer, he built this system according to the datasheet and following the steps in Collin Wells' technical blog in the link below.
https://e2e.ti.com/blogs_…