Part Number: XTR300EVM Other Parts Discussed in Thread: XTR300 , XTR111 I am new to using these types of devices and am trying to get a simple test set up to explore the features of them. When following the documentation for the device it calls for a two…
Part Number: XTR300EVM Other Parts Discussed in Thread: XTR305 , , XTR300 Hello ladies and gentlemen,
for a new project (0-20mA output at a load cell) we want to use the XTR305 in the future.
Now I have the evaluation board of the XTR300 (XTR300EVM), which…
Part Number: XTR300EVM Other Parts Discussed in Thread: XTR300 , , OPA192 , OPA2192 I'm seeing significant broadband noise on the output of the EVM. Is there a recommended approach for filtering the output without creating a large stored energy reservoir…
Part Number: XTR300EVM Other Parts Discussed in Thread: XTR300 , I've been able to get a voltage output using a PWM using the Evaluation Module however, have not been able to get a current output. The voltage Also has not been perfectly accurate from the…
Part Number: XTR300EVM Dear E2E,
Good Day!
We just wanted to check if there's any other schematics with better quality image of XTR300EVM? We found one in the user's manual, but it's hard to read.
http://www.ti.com/lit/ug/sbou034a/sbou034a…
Hi Kashyap,
There is a typographical error on the input impedance specification of instrumentation amplifier (IA) of the XTR30x data sheets. The error in the data sheet spec was copied into the SPICE model providing the erroneous simulation results. The…
Part Number: XTR300EVM Other Parts Discussed in Thread: XTR300 I am testing the XTR300 voltage to current amplifier for possible use in application where a +- 10V signal will be converted to a +- 20mA signal that will be driven through a 100-1000 Ohm…
Other Parts Discussed in Thread: XTR300EVM , XTR300 Good day friend, I bought XTR300EVM with oldest version, and I was confused because the evaluation board is different with in the datasheet. Please could someone help me to set the jumper, because there…
Part Number: XTR305 Other Parts Discussed in Thread: XTR300EVM , XTR300 Hello,
I've this circuit of XTR305 for Analog Output. Even if the output for DAC which is input to XTR305 is there, still XTR not giving output.
Below is the circuit I've prepared…
Part Number: XTR300 Other Parts Discussed in Thread: XTR305 , , TIPD155 Dear TI Team Our customers are requesting Vin vs Vout measurement data when using the XTR300 and XTR305 in voltage output mode. (To understand the error of Vout with respect to Vin …