Part Number: ADC128S102EVM
Hi E2E,
Good day.
We have a customer asking for the board size of ADC128S102EVM . Hope you could support us on this inquiry
ADC128S102EVM:
www.ti.com/.../ADC128S102EVM
Thanks.
Part Number: ADC128S102EVM I need to interface to the ADC128S102EVM board through the J26 SPI port
Can I use the Precision Host Interface board as just a power supply and voltage reference?
Can I just plug in the USB but not connect using the Control…
Part Number: ADC128S102EVM I have two versions of the ADC128S102EVM board: a small one we bought a year ago and a much larger one where all the inputs are broken out to SMA connectors.
I can plug the old style ADC128S102EVM directly to an Arduino Due…
Part Number: ADC128S102EVM Dear TI:
Could you please post a link to a high quality copy of the schematic for the new revision of the ADC128S102EVM board, please? Thanks!
Part Number: ADC128S102EVM Other Parts Discussed in Thread: MSP430FR5969 I start the MSP430FR5969 launchpad in debug mode set a voltage (<1.5V), using an external source, on one of the analog inputs (usually the buffered input 3). The read voltage via…
Part Number: ADC128S102EVM The software accompanying the ADC128S102EVM requires installation of an unsigned USB driver in order to work, but Windows 10 prevents such installation. Is a signed version of this driver available? If not, what is the recommended…
Part Number: ADC128S102EVM The ADC128S102EVM pin description thread had an answer that stated: "If you have VA set to 5V, you can use IN4 and IN5 with inputs up to 5V. IN0 - IN3 and IN6 are limited to 3.3V because of the op amp that is in the signal path…
Part Number: ADC128S102EVM Other Parts Discussed in Thread: ADC128S102 I am using the ADC128S102EVM to evaluate the ADC128S102 and I am experiencing crosstalk between channels.
My test setup is fairly simple.
I have connected the EVM board to an STM32F7…