Other Parts Discussed in Thread: ADS4125 Hi,
I am just trying to track the pins of FPGA used to interface with ADS4125EVEM.
I am surprisingly finding that, TRUE o/p of ADS4125 is connected to COMPLEMENT i/p of FPGA.
Example:
Differential
ADS4125
…
Other Parts Discussed in Thread: DAC3152EVM , TVP5146 , ADS4125 Hi DSP Experts,
I am generating a sine wave of 5Mhz frequency using TSW1400 and DAC3152EVM and I am getting an expected o/p at transformer output.
Now I want to see, how this sine wave is sampled…
User,
Is this a problem with a custom board you built that has the ADS4125 or are you using the TI ADS4125EVM? I cannot tell by your description. In either case, I would check the following:
1. Voltages to the ADC are correct.
2. The registers are programmed…
Part Number: ADS4125 Hello,
Is the evaluation board of ADS4125 is ADS4125EVM ?
Does ADS4125EVM connect to TSW1200 ? We already have TSW1400 can it also fit?
Thanks,
Inbal
Other Parts Discussed in Thread: ADS4122 Hi,
I am using ADS4122 in my card and I am surprisingly observing that MSB is toggling even though ADC has no analog input.
The differential input at ADC shows 0V on oscilloscope.
I thought there might be something…
A quick search of the product information shows that TI manufactures 17 active A/D converter ICs with 12 bits of resolution and sampling rate limits of 105 to 250 MSPS, typically with LVDS output. They have evaluation modules, e.g. ADS4125EVM, but these…