Part Number: ADS4246EVM Dear TI,
I would like to request the FPGA code for ADS4246EVM chip using vivado IDE.
I use zynq 7000 chip in my project.
Thanks.
Regards,
Thiha
Part Number: ADS4246EVM We are using the ADS4246EVM connected to a Xilinx Artix-7 FPGA as a development system whilst our hardware is ready.
As a medical company, we need to make sure the ADS4246, via the SPI, has been programmed correctly. Therefore,…
Part Number: ADS4246EVM
We are using the ADS4246EVM connected to a Xilinx Artix-7 FPGA as a development system whilst our hardware is ready.
As a medical company, we need to make sure the ADS4246 , via the SPI, has been programmed correctly. Therefore, after…
Part Number: ADS4246 We are planning to use the TSW1400EVM card to capture the ADC outputs from an ADS4246EVM ADC evaluation board.
Do I understand correctly that the HSDC Pro v5.00 software controls both the capture card and the ADC?
Part Number: TSW1405EVM Hi Team,
Our customer would like to use replace the TSW1405EVM with Artix-7 FPGA. According to our customer,
I bought an ADS4222EVM board+TSW1405EVM. I tested the EMVs, and they worked very well. Now, I would like to replace TSW1405EVM…
Hi,
We do not have reference code for the Spartan 6 or other FPGA development platforms. However, we do have partnership with Avnet for the ML605 + TSW4200 Speedway Demonstration Kit, and the ADC EVM in that kit has the same FPGA interface as the ADS4246…
Part Number: ADS4246 thanks for your answers so far :-
We are going to capture 2 channels from the ADS4246EVM with the TSW1400 and save the data in binary format (since it will be 1Gbyte).
I presume that the samples in the binary file alternate, ch0…
Part Number: ADS4246 My eval boards ADS4246EVM with the TSW1400 have arrived and I am trying to get the system up and running but need some help.
The instructions are to start the software, select the 422x ADC and when prompted to upload the firmware…