Hi,
ray yang said: Is there a tool to recreate them
I find this online AES calculator. You can do your own searches and find other tools.
https://www.devglan.com/online-tools/aes-encryption-decryption
Part Number: MSP430F2617 Other Parts Discussed in Thread: AES-128
I'm looking to implement AES-128 GCM to secure a communication interface between two MSP430 devices.
I was able to find another AES-128 ECB implementation provided by TI at https:/…
Part Number: TM4C1294NCPDT Hi, I am using TM4C129 micro, I want to use its hardware aes engine. my aes mode is CFB128 bit. I have two questions. 1. does the hardware aes engine support variable length data? for example, can I encrypt 20 bytes, then decrypt…
Part Number: MSP430FG4616 Other Parts Discussed in Thread: AES-128 Dear expert,
Do we have AES-256 open source for this msp430 device?
If not, may you share any other security for encryption/decryption on MSP430FG4616.
Hello,
Using SDK8.6, not using SDK9.1 testing, currently found on SDK8.6:
1. Using the openssl speed command to test the algorithm performance, it is found that the speed of using software to process encrypted data is much faster than that of hardware…
Part Number: PROCESSOR-SDK-AM62X Hello,
We follow the link provided below to build and implement the hardware crypto accelerator supported on the AM62X platform. The hardware crypto accelerator driver exists and is loaded, but the hardware acceleration…
Hi Hong
Thank for you reply, I follow the Linux kernel cryto driver reference, and insmod the ko, but it can't work, report lib error:
Invalid engine "devcrypto" C0CFF8B6:error:12800067:DSO support routines:dlfcn_load:could not load the shared…
Part Number: LAUNCHXL-CC26X2R1 Hi,
I am working on CC26x2R1 BLE SoC. My use case is to decrypt the data with 128 bit. Key and IV length is 16 bytes and Input data is 24 bytes.
I am following these steps:
static uint8_t AES_Decrypt_Key(uint8_t const …
Hi Jun, I have a question about the AT command of cc3235MODSF.
WiFi Frequency: 5GHz
WiFi authentication method
- Authentication protocol: 802.1x authentication
- Linkage method: WPA2 Enterprise
- Authentication method: EAP-PEAP MSCHAPv2
- Encryption: AES…