Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-CC2650MA , LAUNCHXL-CC2640R2 , CC2340R5 Hi,
I would like the ability to flash firmware updates wirelessly to the LaunchXL-F28379D/ TMDSCND28379D.
I have the following questions:
Can…
Part Number: EVM430-FR6047 Other Parts Discussed in Thread: BOOSTXL-CC2650MA , , CC2650 Hello Guys,
Good day.
Is BOOSTXL-CC2650MA compatible with EVM430-FR6047?
Our customer need Bluetooth 4 with the EVM module. If the CC2650 doesn't work, do you have any…
Part Number: BOOSTXL-CC2650MA I've successfully ported the updated github version of the SPP_BLE_Server project to the BOOSTXL-CC2650MA, and essentially want the serial data attributes without the status or config attributes. My initial approach was…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: SYSBIOS Starting with the updated SPP_BLE_Server example from Github, I have two separate tasks I've added, one of which loops with a variable delay for Task_sleep() blocking it for a bit at…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: CC2650 CCS: 10.4
XDC: tirtos_cc13xx_cc26xx_2_20_01_08
SDK: ble_sdk_2_02_01_18
Compiler: ti-cgt-arm_5.2.6
I'm (still) working with the updated serial port profile example from Github, and I…
James Morris said: The definition of __TI_COMPILER_VERSION or __TI_COMPILER_VERSION__ alters the prototype of ltoa() in osal.c
The definition of the function ltoa changed between compiler versions 5.2.6 and 20.2.5.LTS. You need to be sure to call it correctly…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: SYSBIOS , CC2650 I am trying to run the simple_broadcaster_cc2650lp example except running with the BOOSTXL-CC2650MA connected to a XDS110 debug probe. (I have modified the project to defi…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: CC2650 , BLE-STACK Hello.
I want to change the firmware of CC2650 Module BoosterPack from UART to SPI. In order to create a SPI-compatible firmware, we did the following. Q1: Is there anything…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: LAUNCHXL-F280049C , CC2650 , LAUNCHXL-CC26X2R1 , SIMPLELINK-CC13X2-26X2-SDK I want to use the boostpack BOOSTXL-CC2650MA with LAUNCHXL-F280049C to achieve wireless communication between two LAUNCHXL…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: UNIFLASH Hi,
I am trying to load program 0 into the MSP4321R with it connected to the CC2650MA by following the instructions on this page: http://dev.ti.com/tirex/explore/node?devtools=BOOSTXL…