Part Number: WL1807MOD Other Parts Discussed in Thread: CC3135MOD Hello expert,
As for WL1807MOD and CC3135MOD
1) How the customer can calibrate the RSSI level?
2) How the customer can calibrate the career frequency?
3) In wl1807mod.pdf datasheet, it…
Hi Naoki
Please see the Interference Mitigation App note in section 3.3.
There is also a training video on interference mitigation.
If there are further queries on this then please open up a new thread.
Regards,
AG
Hello,
I tried this out in my environment, but I didn't see a way to do this for two different processor families. I'll need to investigate further.
Note that both the devices and CCv4.10 is extremely old and unsupported, hence it may take a bit…
Hi,
I received the following question from my customer.
There is figure 7 on the snlu099A.
My customer would like to calculate manually by themselves.
Could you tell me setting of SPAN and RBW on the the spectrum analyzer observing career spectrum?
…
Other Parts Discussed in Thread: TLC5955 , TLC59116 Most needed device in my entire career still doesn't seem to exist, but I could be wrong.
This situation keeps coming up, again and again. I have 20 LED's to drive (actually 40, but I have two common…
Dear All,
I'm currently a masters student in Rutgers University studying Electrical Engineering, and I want to one day become an analog design engineer and design op-amps, amplifiers, PLL etc.
Now Rutgers University is not a good school for those…
Looking for a career change. Currently a CNC machinist/programmer but the oil and gas industry isn't looking too well imo. Wondering if anyone with experience in the IT Computer Science field can point me in the right direction. (For instance, if I want…
Hi, Thanks for your response,
Input voltage = 2.6 to 3V (power source: 2 x D size Alkaline batteries). Output current: 7uA to 70mA
The input voltage was stable during all of those measurements.
I know the light SHOULD not change anything, but that what…
Hi Daniele,
Thanks for letting us know! Yeah, I tried another couple of times to reproduce it and I was not successful.
Okay, thanks for the update. If they have the link to this thread, I encourage them ask related question (using the orange button at…
Hi,
sorry for the late reply. I have shared the schematic PDF and screenshot of relevant portions of the layout in the personal messages. The VDS spikes were due to some ringing in the miller plateau of the gate drivers which crossed Vth of the FET. We…