Part Number: TMDSCNCD2800157 Hello,
We just received our new dev board and are trying to get some simple programs running as to test the system/environment, however we are unable to flash/debug the system. When we first tried to run the debug session…
Part Number: IWRL6432BOOST the DIP switch on my board: S1 swich to ON-ON-OFF-OFF-ON-ON and S4 OFF-OFF-OFF-ON
but the CCS report error on start debugging
Part Number: CC2340R5 Dear TI,
Can I run Debug mode without flashing any program (as well as erase chip)? Does Debug configuration support any setting that allow us to disable this step?
My CCS Studio Version :
Version: 12.6.0.00008
Thanks,
Zach
Part Number: MSPM0G1507 Other Parts Discussed in Thread: LP-MSPM0G3507 , My CCS Theia 1.2.0 debugger was working earlier today and I was able to launch debug sessions of my application code running on breadboard prototype hardware (MSPM0G1507 MCU) using…
Part Number: IWR6843AOP
Hi,
I'm trying to debug the DSS side of the 3D_people_count_68xx project. I created a group debug and started debugging and connecting to both cores.
I could set and use breakpoints in the MSS project but debugging information…
Part Number: AM6421 Hi team,
I am using Processor-SDK-Linux-RT-AM64x. Actually, I have installed CCS on Linux and doing a cross compilation. The binary is loaded into the SD card, and we run it when the LINUX boots up from SD card. Can you please help…
Hi Henley,
Kenley said: DAP Connection Error. This could be caused by the device having gone to low power mode.
This means PC cannot recognize the M0 DAP which is used for debug and further for factory reset.
What CCS version is customer using right now…
Part Number: IWRL6432 Hello experts,
The related question describes a manual method of doing rapid debugging on the IWRL6432. In the past I found a file called 6837.launch_iwrl6432.js which was a script that dramatically increased the debugging iteration…
Hi,
Gibbs Shih said: (1) Vision app do not allow CCS debugging? (y/n)
By debugging the application, do you mean step wise execution of the A72 vision_apps application using CCS?
Then no, it is not supported on CCS.
Gibbs Shih said: (2) Evan SBL/SPL boot…